Robotics
  • Technologies
  • More
Robotics
Forum Wire and Cable Basics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 76 subscribers
  • Views 1066 views
  • Users 0 members are here
  • cable
  • electrical
  • installation
Related

Wire and Cable Basics

e14 Contributor
e14 Contributor over 16 years ago

Basic installation of wire & cable can have a major impact on how long the cables will last.  If you are installing cables on a welding robot, in a tray or cable reel, following some basic guidelines will always help.

 

1) Allow the cable to hang freely for 24 hours is possible, this will allow any tension in the cable to be released.  Tension is imparted to the cable by pulling on the jacket.  Typically, when cables are spooled onto a cable reel there will be some type of pulling which can cause this tension.

 

2) Do not exceed the cables rated pull tension.  This type of information will vary from cable to cable, if you don't know the cables rated pull tension you should consult with your cable supplier.  Exceeding this rating is one of the fastest ways to "kill" a cable.  The conductors will get pulled out of their lay and begin to sprial or "corkscrew".  This is the first sign of a problem.

 

3) Do not exceed the cables bend radius.  This is typically determined by multiplying the outside diameter of the cable by a factor to determine the minmum bend radius.  Static cables which will not be flexed once installed can usually have a minimum bend radius of around 5 times the overall OD of the cable.  Cables which will be flexed when installed have a bend radius of anywhere from 6-10 times the outside diameter.  Again, if you aren't sure you should consult your cable supplier.

 

4) Use a mesh strain relief at both ends of the cable if possible.  This will help spread the load of the jacket of the cable and prevent jacket stretch and pressure on the conductor bundle.

 

Each application will be slightly different but these basics will be a good start to improving the live of your electrical wire.  For more information you can go to http://www.tpcwire.com.

Attachments:
imageCable Guide.pdf
  • Sign in to reply
  • Cancel
Parents
  • ratsept
    ratsept over 16 years ago
    I also work with welding robots and one more thing to observe is that not all cables are UV resistant and intense light from the welding arc can and will destroy some cables. The best solution is usually to run all application specific cabling inside the manipulator arm if at all possible. It will be a pain to install and/or replace but will save a lot of money and downtime if done right. Most robots also have all the cabling in sections and when putting in application specific cabling it is a good idea to use the same principle. Never put welding power cables in the same bundle with signal cables - believe me, I speak from experience.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ratsept
    ratsept over 16 years ago
    I also work with welding robots and one more thing to observe is that not all cables are UV resistant and intense light from the welding arc can and will destroy some cables. The best solution is usually to run all application specific cabling inside the manipulator arm if at all possible. It will be a pain to install and/or replace but will save a lot of money and downtime if done right. Most robots also have all the cabling in sections and when putting in application specific cabling it is a good idea to use the same principle. Never put welding power cables in the same bundle with signal cables - believe me, I speak from experience.