Robotics
  • Technologies
  • More
Robotics
Forum New robot to give sponge baths
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 75 subscribers
  • Views 810 views
  • Users 0 members are here
  • robots
  • embedded
  • development
Related

New robot to give sponge baths

Eavesdropper
Eavesdropper over 16 years ago
image
 
Robots have been known to have some remarkable skills. They can have discussions with us, help us move heavy loads, and more recently have even become ethical. But we’ve never really heard of a robot that has a gentle touch, much less one that has a gentle enough touch to give patients a sponge bath. It brings up a certain fear of the robot ‘sponging’ the patients skin clean off. However this fear is unprecedented and totally warrantless when it comes to Cody. A team from the Georgia Institute of Technology, led by Dr. Chih-Hung (Aaron) King, has designed the robot to help hospitals their bed bath duties. Cody is outfitted with specialized arms to witch one of them has a bath mitt attached. The robot identifies a portion of the patient’s skin that needs cleaning using a built in camera and a laser range finder. After the portion of dirty skin is found the robot proceeds to clean in a gentle wiping motion using equilibrium point control that removes up to 96% of grime in the target area. Cody also has a few safety protocols built in so it doesn’t accidentally cause pain or damage a patient when it’s performing its duties such as a reduction in arm stiffness, a program that is designed to limit Cody’s pressure when cleaning, and even has a stop button in case the robot gets out of control.  The initial benefits Cody would have to patients are quite useful, such as privacy and a greater sense of independence. Psychological effects of using a robot on patients are not entirely known as of yet but Dr. King used Cody in a demonstration and at first felt nervous at first but the tension he experienced faded after a short period of time and at no time was he ever afraid. As it stands now the robot needs a human counterpart to help identify and clean potential patients using a remote-control unit, but future versions will be totally autonomous. I can see where having privacy is important especially when sponge baths are usually felt as an embarrassing and demeaning moment, but on the other hand sometimes a human touch is more important and creates a sense of care a robot just can’t provide.
 
Eavesdropper
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    I think we are still a fair way from having a robot operate completely autonomously with something as fragile as the human body on a day-to-day basis, the main problem that I see comes down to who gets the blame if it all goes wrong and my poor nan gets her eye poked out!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Eavesdropper
    Eavesdropper over 16 years ago in reply to e14 Contributor

    I agree. Robots follow programming, and if no fail safes are put in the system, they will execute the code with disregaurd for any other factor. Including the a human it's handeling. I will wait for version 2 or 3 before I get the "bot-massage."

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Eavesdropper
    Eavesdropper over 16 years ago in reply to e14 Contributor

    I agree. Robots follow programming, and if no fail safes are put in the system, they will execute the code with disregaurd for any other factor. Including the a human it's handeling. I will wait for version 2 or 3 before I get the "bot-massage."

     

    E