Robotics
  • Technologies
  • More
Robotics
Forum 今年67%以上大尺寸液晶面板将采用LED背光
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 75 subscribers
  • Views 169 views
  • Users 0 members are here
Related

今年67%以上大尺寸液晶面板将采用LED背光

YYD
YYD over 15 years ago
来源:电子产品世界
     
  据IHS iSuppli公司,2011年全球出货的三分之二以上大尺寸液晶面板将采用LED背光,该比例2010年低于50%。
  预计2011年将有67%的大尺寸液晶面板采用LED背光,高于2010年的44%。2011年LED背光大尺寸液晶面板出货量将达到4.956亿块,比2010年的2.833亿块大增74.9%。
  对于笔记本电脑和上网本面板,2011年LED背光的占有率将从2010年的91%上升到100%。2011年LED背光在电视和监视器面板中的占有率将从2010年的20%左右上升到接近50%的水平。
  到2014年,LED背光大尺寸液晶面板的出货量将从2009年的1.178亿块增长到8.346亿块,期间的年度复合增长率为47.9%。
  下图所示为IHSiSuppli公司对2009-2014年大尺寸LED背光液晶面板出货量的预测。IHSiSuppli公司对大尺寸液晶面板的定义是,对角尺寸大于等于10英寸的面板。
 
  LED背光面板2010年成为推动大尺寸液晶面板出货量增长的主要因素,是增长最快的领域,而且很快成为液晶市场的最大领域。随着成本不断下降,消费者对于LED背光电视的需求越来越强,更多的消费者青睐其出色的画面质量、较低的功耗和更薄的外形。
  面板供应过剩隐忧
  尽管LED背光产品出货量强劲增长,但2011年大尺寸面板市场面临供应过剩的隐忧。供应过剩将导致价格下滑。
  根据对面板供应商当前生产计划的分析,2011年上半年产能可能明显超过市场需求。但是,2011年下半年产能扩张速度可能下降到低于需求的水平。
  如果面板供应商能够明智地控制生产,则2011年液晶产业的情形可能非常不错。同样,上半年过度生产可能导致2011年库存增加和供应过剩。
  2011年3D面板变化
  除了LED背光,2011年大尺寸液晶市场的另一个主要趋势将是3D电视面板市场的转变。2010年3D电视的市场接受情况逊于产业的预期,部分原因是面板和电视机的成本较高。
  许多面板供应商2011年计划推出使用相位延迟薄膜技术的3D电视,不再使用目前的快门眼镜技术。相位延迟薄膜技术与由偏振器薄膜构成的3D眼镜配合使用,这种眼镜的重量较轻而且成本较低。采用该技术,眼镜成本约为10美元,使消费者更容易拥有多副眼镜。快门眼镜的成本为100美元。
  除了成本较低,相位延迟薄膜技术据称串扰也较低,而且亮度可能高于采用快门眼镜技术的面板。它也可以与较低的帧速率(60Hz),甚至CCFL背光配合使用,从而可打造较低端的、价格较低的3D电视。但是,快门眼镜技术具有分辨率较高的优势,而且具有垂直视角较宽等其它一些优点。面板供应商和一些品牌厂商,尤其是中国企业,希望在2011年推出成本较低的相位延迟薄膜技术和偏振器眼镜,以提高3D的占有率。