Robotics
  • Technologies
  • More
Robotics
Forum vision guided robot  using android and arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 77 subscribers
  • Views 1606 views
  • Users 0 members are here
Related

vision guided robot  using android and arduino

e14 Contributor
e14 Contributor over 13 years ago

i am doing vision gudied robot with arduino and android through bluetooth communication . i have done the image processing part using andriod.But i am facing problems in image processing. The colored image is getting transformed to black and white image. but the code that is written to detect the black tape is not working properly.. Could some one help me to debug.

 

 

public class DrawOnTop extends View

{

          BtConn btcon;

          //Display

          Bitmap mBitmap;

          Paint mPaint;

          int mImageWidth, mImageHeight;

 

          //Frame data

          byte[] mYUVData;

          int[] mRGBData;

          int[] mBWData;

 

          //FPS

                    long lastFrame = System.currentTimeMillis();

 

                    //PID

                    float proportional;

                    float integral;

                    float derivative;

                    float last_proportional;

                    int Kp=1;

                    int Kd=2;

                    int Ki=0;

 

                    //Motor Controls

                    int right_speed=0;

                    int left_speed=0;

                    int max_speed = 255;

 

          //Line Tracking

          static int tracking;

 

          int minPixels = 10;

          int threshold = 60;

          int tapeCenter;

    public DrawOnTop(Context context) {

        super(context);

 

        // Start off PAUSED

        tracking = 0;

 

        mPaint = new Paint();

        mPaint.setStyle(Paint.Style.FILL);

        mPaint.setColor(Color.RED);

        mPaint.setTextSize(25);

 

        mBitmap = null;

        mYUVData = null;

        mRGBData = null;

    }

 

 

    @Override

    protected void onDraw(Canvas canvas) {

        if (mBitmap != null)

        {

                  int canvasWidth = canvas.getWidth();

                  int canvasHeight = canvas.getHeight();                         

 

                  grayscaleToBlackWhite(mRGBData, mYUVData, mImageWidth, mImageHeight,canvas);

                  int tapeCenter=DetectingArea(canvas,mRGBData, mImageWidth, mImageHeight);

 

                  //PID

                        proportional = tapeCenter - mImageHeight/2;

                        integral = integral + proportional;

                        derivative = proportional - last_proportional;

                        last_proportional = proportional;

                        int lineError = (int)(proportional * Kp + integral * Ki + derivative * Kd);

 

                        // Restricting the error value between +/- max_speed.

                        if (lineError< -max_speed)

                        {

                                  lineError = -max_speed;

                        }

                        if (lineError> max_speed)

                        {

                                  lineError = max_speed;

                        }

 

                        // If error_value is less than zero calculate right turn speed values

                        if (lineError> 0)

                        {

                        right_speed = max_speed + lineError;

                        left_speed = max_speed;

 

                        }

                        // If error_value is greater than zero calculate left turn values

                        else

                        {    

                    right_speed = max_speed;

                        left_speed = max_speed - lineError;

 

                        }    

 

 

                        int[] data = new int[3];

                        data[0] = 0; //Forward

                        data[1] = right_speed;

                        data[2] = left_speed;

 

 

                  long curFrame = System.currentTimeMillis();

                  float fps = 1000/(curFrame - lastFrame);

                  lastFrame = curFrame;

 

 

 

 

                  // Draw bitmap

                  mBitmap.setPixels(mRGBData, 0, mImageWidth, 0, 0, mImageWidth, mImageHeight);

                  Rect src = new Rect(0, 0, mImageWidth, mImageHeight);

                  Rect dst = new Rect(0, 0, canvasWidth, canvasHeight);

                  canvas.drawBitmap(mBitmap, src, dst, mPaint);

 

 

 

 

 

                  canvas.rotate(-90, canvasWidth/2, canvasHeight/2);

                  mPaint.setTextSize(25);

                  canvas.drawText(mImageWidth + "x" + mImageHeight, 200, -140, mPaint);

                  canvas.drawText("fps: " + fps, 500, -100, mPaint);

 

 

        }

        super.onDraw(canvas);    

    }

 

 

 

 

    public void grayscaleToBlackWhite(int[] rgb, byte[] yuv420sp, int width, int height, Canvas canvas)

    {

 

              final int frameSize = width * height;

 

              mPaint.setTextSize(25);

 

 

              for (int pix = 0; pix < frameSize; pix++)

              {

                        int pixVal = (0xff & ((int) yuv420sp[pix])) - 16;

                        if (pixVal < threshold)

                        {

                                  pixVal = 0;

                        }

 

 

                        else

                                  pixVal = 255;

                        rgb[pix] = 0xff000000 | (pixVal << 16) | (pixVal << 8) | pixVal;

 

 

              }

             

 

    }

  public int DetectingArea(Canvas canvas,int rgb[],int height, int width)

  {

 

            int start=-1;

            int stop=-1;

            int tmpStart=-1;

            int tmpStop=-1;

          int scanline=-1;

            for(int i=0;i<width;i+=10)

            {

 

                                for(int j=0;j<height;j++)

                                 {

                                          //check for black line only.

                                          //find all black line centres and compare with the centre of the screen

                                          int pixVal = (0xff & (int) rgb[i+j*width]);

 

                                          if (pixVal == 0)

                                                      {

                                                              if(tmpStart==-1)

                                                              {

                                                                        tmpStart=j;

                                                              }

                                                              else

                                                              {

                                                                        tmpStop=j;

                                                                        if(tmpStop-tmpStart>minPixels &&

                                                                                            (Math.abs((tmpStop-tmpStart)/2 - height/2)

                                                                                            <  Math.abs(stop-start)/2 - height/2))

                                                                        {

                                                                                  start=tmpStart;

                                                                                  stop=tmpStop;

                                                                                  scanline=i;

                                                                        }

                                                                        else

                                                                        {

                                                                                  tmpStart=-1;

                                                                                  tmpStop=-1;

                                                                        }

                                                              }

 

                                                      }

                                 }

 

            }

            if (start > -1 && stop > -1 && scanline >-1) {

                        for (int pix = start; pix <= stop; pix++) {

                                        rgb[scanline+pix*width] = 0xff000000 | (0 << 16) | (255 << 8) | 0;

                        }

            }

 

 

            return (start+stop)/2;

 

  }

}

  • Sign in to reply
  • Cancel
Parents
  • Ramu
    Ramu over 13 years ago

    And why do you want to seperate black region to other frame? T think the easyest way is to set the camera that botom will see near the robot front, ant top of the screen some centimeters avay.

    Then i think of 2 ways:

    1 - manualy look for begining and ending of a black kolor in one line. if its center is in center, then you are in the right place. And scan 10 lines of all lines, or less. if the screen is 64x64 then scan every 6 lines. If you get that all lines have black in the center, you go top speed, if lovest line is in center, and hier line has black going to sone side, then start turning. And so on.

    2 - use edge detectin, and based on the corners get some lines. And based on lines positions and oriantations you can decide how to go. but this is harder, because bended lines will make a lot of short stait linesor in some realy bended ones, you may get no strait lines. so i think 1rst option is more easy one.

     

    Or you can try to detect a center of all black line in the screen and then decide how to go. this has a problem if you have a road fork, it will not tell you that. it vil calculate center in betwean them.

     

    and before looking for a black line, you may want to filter out small black parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Ramu
    Ramu over 13 years ago

    And why do you want to seperate black region to other frame? T think the easyest way is to set the camera that botom will see near the robot front, ant top of the screen some centimeters avay.

    Then i think of 2 ways:

    1 - manualy look for begining and ending of a black kolor in one line. if its center is in center, then you are in the right place. And scan 10 lines of all lines, or less. if the screen is 64x64 then scan every 6 lines. If you get that all lines have black in the center, you go top speed, if lovest line is in center, and hier line has black going to sone side, then start turning. And so on.

    2 - use edge detectin, and based on the corners get some lines. And based on lines positions and oriantations you can decide how to go. but this is harder, because bended lines will make a lot of short stait linesor in some realy bended ones, you may get no strait lines. so i think 1rst option is more easy one.

     

    Or you can try to detect a center of all black line in the screen and then decide how to go. this has a problem if you have a road fork, it will not tell you that. it vil calculate center in betwean them.

     

    and before looking for a black line, you may want to filter out small black parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Ramu

    Thank you,

       The image proceesing part is done.I didnt use edge detection. i used the first way.But how to send these data to arduino board so that my robot can move.I mean what hardware and software should i usefor communication through bluetooth. My robot have to move through the black line .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Ramu

    Actually i need to avoid white line and not black. I am not doing a line follower. I am ding a robot which will move forward with in a boundary and by avoiding the obstacles.The boundary line may be of black or white.Robot should not cross the buondary. As first step to my project i am trying to do a line follower.So that i could get knowledge about image processing and communication part which makes it easy to my original project