Robotics
  • Technologies
  • More
Robotics
Forum raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 78 subscribers
  • Views 806 views
  • Users 0 members are here
Related

raspberry pi

rhydian98
rhydian98 over 13 years ago

Could i use raspberry pi to make the robot move and program the different movements?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I haven't had the opportunity to actually work with a Raspberry Pi as of yet, but I have done quite a bit of research into it. It would be nice to use in robotics, but I wove to agree with Raimondas Klemka, a microcontroller would probably work better for the application. Possibly the most popular, and easiest to use (at least in my experience), is the Arduino. If you havent already, I would suggest looking into an Arduino Mega, which offers plenty of pins, for plenty of connections. Another bonus with the Arduino is how easily it can be embedded into your project.

    Maybe you could use the Pi to program an Arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ramu
    Ramu over 13 years ago in reply to e14 Contributor

    Yes for controlling something microcontrolles liek arduino mega are better somimes, because the have a lot of pins and some of the processin can be made by microcontroler, and other stuff can be processed by Pi. but Pi can be used for simple computer vision, for controlling arduino over usb and other stuff. but if you need just few I/O then Pi is good to image But consider on thinking of usin 2 or more procesosrs, because sometimes it is better to have few less loaded processors or microcontrollers, then to putt it all in one and run it on the limit.

    Now I'm thinking on using pi for wifi data transmission. And if it is posable to stream video over 3g network. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Ramu

    You might want to consider using one of these. ( http://wyolum.com/projects/alamode/ )

     

    The RaspberryPi can provide the processing and then hand of the control bit to the Arduino.

    You can utilise the wide variety of shields to do the motor control.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Ramu

    the pi looks to be a good platform for robot control ,  the power to network beeing its main advantage over microcontrolers ,

    although usb bandwidth is more of an issue onece you start messing about with video

     

    to handle  3g ( usb dongle ) + 2 webcams  needs a controler with  at least 3 individual host usb ports   not a single host usb port and a hub

    as the usb bandwith falls over when running eather  3g and video or twin video

     

    should you be able to streem 2 video feeds over wifi or 3g/4g  link  then you could offload the video to a remote PCL (point cloud library) server cluster providing sterio webcam to 3d mapping  in real time

     

    although looks like  itx pc's or laptop with a network link to a 16 core 3ghz xeon cluster is the way to go

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Ramu

    the pi looks to be a good platform for robot control ,  the power to network beeing its main advantage over microcontrolers ,

    although usb bandwidth is more of an issue onece you start messing about with video

     

    to handle  3g ( usb dongle ) + 2 webcams  needs a controler with  at least 3 individual host usb ports   not a single host usb port and a hub

    as the usb bandwith falls over when running eather  3g and video or twin video

     

    should you be able to streem 2 video feeds over wifi or 3g/4g  link  then you could offload the video to a remote PCL (point cloud library) server cluster providing sterio webcam to 3d mapping  in real time

     

    although looks like  itx pc's or laptop with a network link to a 16 core 3ghz xeon cluster is the way to go