Robotics
  • Technologies
  • More
Robotics
Forum Arduino Motor Control
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 80 subscribers
  • Views 1797 views
  • Users 0 members are here
Related

Arduino Motor Control

e14 Contributor
e14 Contributor over 13 years ago

Can someone please tell me to control a motor using an arduino. I want to begin a robot project.

  • Sign in to reply
  • Cancel
  • billabott
    billabott over 13 years ago

    @JacobL

    A good place to start would be: http://www.arduino.cc/en/Tutorial/StepperBipolar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    I have some old 3.5 floppys and some old CD drives. Will these motors work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago

    This tutorial is probably the easiest place to start:

    http://www.oomlout.com/oom.php/products/ardx/circ-03

     

    Also check out their relay tutorial which uses a relay, instead of a transistor, to control a motor.

     

    If the motors are simple 2-wire motors, then yes those will work with the tutorials I pointed to. If they have more wires, the tutorial Billabott pointed to will be the one to use.

     

    I've also used the little motors from power toothbrushes (crest spinbrush was one).

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ramu
    Ramu over 13 years ago in reply to e14 Contributor

    About Floppy and CD-ROM motors, there are few diferent ones there. For example center one (spinning the floppy and CD/DVD usualy it is BLDC motor). It is the hardest to controll motors in thies devices. manualy controll them it is bit hard. but in PCB there should be drivers. Not shure how the drivers are controled, but it shold be eacyer. by the way FLOPPY and CD-ROM BLDC (Brushless Direct Current) motors may be part of the PCB, because they usualy have Hall efect sensors to now the current possition. Then In floppy there is a SEPPER mottor moving the data reading head. it usualy has 4 wires. And they can be controlled by arduino, but you have to use some transistors or with STEPPER controller microchip. They make the weak arduino signal in tu strong one, sutable to drive the mottor. There is an explanation how to controll 6 wire and 4 wire STEPPER motor: http://nerdclub-uk.blogspot.com/2011/09/stepper-motor-control-2-phase-4-phase.html

    Then in CD-ROM there is a regular DC motor with only 2 wires. They are the simplest to control. Just connect the pover (+ and - ) to the wires and it goes. If you swap the + and -, then it will go to the other side. Non revesable DC mottor speed controll with arduino and a transistor http://arduinoarts.com/2011/08/arduino-tutorial-f1-rc-car-dc-motor-driven-by-mos-transistor/ the potensiometer is just for telling arduino how fast you want it to go.

     

    There are stepper mottor or 2x DC mottor controolers like this: http://www.ebay.com/itm/Stepper-Motor-Drive-Controller-Board-Module-L298N-for-arduino-NEW-good-/330808982986?pt=LH_DefaultDomain_0&hash=item4d05c07dca if you do not know how to use it, please ask. I like thies, because it is realy simpple and fast to controll small motors upt to 2A (look on the mottor or in its datasheet how much amps does it use).

     

    And what type of mottors to use it depends on what the robot is going to do ant in what part. If it is for driving weals, it would be better tu use DC image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ramu
    Ramu over 13 years ago in reply to Ramu

    And for making bigger robot and controlling more powerfull robots I like this: http://www.parallax.com/StoreSearchResults/tabid/768/txtSearch/HB-25/List/0/SortField/4/ProductID/64/Default.aspx

    It is realy powerfull one, hade acidently shorted the output, but it is still alive. image we are using them in our robot:

    This robot is made by KTU PI (Kaunas University of Technology Panevėžys Istitution) university students. Not the best robot, but it is our first on.

    image

    Ant this is a video how this robot can use webcam and computer vision application with OpenCV librray to detect an object, take it and bring it back image By the way, in this video motors are replaced with more powerfull ones (from car windshield wipers) to drive outside image

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    So just some fun stuff to get you more motivated to make your own robot image

    If this video is not working, then you can see it in youtube: http://www.youtube.com/watch?v=phI0wMpWMiE

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    The answer to this question really depends on what kind of motors you plan on using. If you're using plain ol' hobby motors or the likes of which that only have two wires, you might consider using an H-Bridge (http://www.robotroom.com/BipolarHBridge.html), which are pretty easy to make and only require a few relatively common parts. I used this method while building a robot arm and it worked well, but it would work even better if you had sensors to track the position of your wheel, arm, or what have you. There are plenty of tutorials across the web for nearly all motor types just a search away.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Ramu
    Ramu over 13 years ago in reply to e14 Contributor

    As a sensor for our robot arm we are using poteniometer, it resolution good for us and it is realy cheap option. Ofcorse you can use encoders, but it is harder to monittor them and they are more expensive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to Ramu

    Search for mod of servo motor to use as a feedback control sensor for really big motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • driverblock
    driverblock over 13 years ago

    Check out Adafruit's Learning System. Plenty of tutorials for controlling motors, steppers, & servos on Arduino and RPi.