Robotics
  • Technologies
  • More
Robotics
Forum How to make a cable to connect to 0.1" dual-row pins?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 75 subscribers
  • Views 888 views
  • Users 0 members are here
  • connector
  • headers
  • cable
  • idc
Related

How to make a cable to connect to 0.1" dual-row pins?

e14 Contributor
e14 Contributor over 11 years ago

I need to make some 10-pin cables to connect my own sensors to a little circuit board called the U-HID, as seen here:

news_board_diag.jpg

The board has male dual-row headers, and are divided into 10-pin (2 rows of 5 pin) blocks, labeled J1, J2, etc. in the image.

 

So, I want to make a little 10-conductor rainbow cable for each position.  I thought perhaps I could use an IDC connector for this, such as

 

http://www.elliottelectronicsupply.com/dual-row-idc-connector-10-position.html

 

...but I'm a little worried that I won't be able to fit two of these next to each other.

 

What do you think?  What's the best way to make a cable/harness to fit each of these 10-pin positions, and still be able to fit them side by side?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Hi Joe, You are correct, most IDC connectors will not fit together. You could use a large 40 pin IDC and peel the ribbon into 10 wire groupings or you could use crimp socket pins in headers which are buttable…
  • jw0752
    jw0752 over 10 years ago +1
    Hi Joe, I have used cables like these in the past to make up some custom connectors. When I want the connector to be integral I use a little glue to connect the individual connectors. http://www.ebay.com…
  • dougw
    dougw over 10 years ago

    Hi Joe,

    You are correct, most IDC connectors will not fit together.

    You could use a large 40 pin IDC and peel the ribbon into 10 wire groupings or you could use crimp socket pins in headers which are buttable.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 10 years ago

    Hi Joe,

     

    I have used cables like these in the past to make up some custom connectors. When I want the connector to be integral I use a little glue to connect the individual connectors.

     

    http://www.ebay.com/itm/T1-3X-40pcs-20cm-Male-To-Male-Female-Dupont-Wire-Jumper-Cable-Arduino-Breadboard-/231708399395?hash=item35f2e59723:g:VHkAAOSw0HVWDsfW

     

    John