Robotics
  • Technologies
  • More
Robotics
Forum Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 79 subscribers
  • Views 1717 views
  • Users 0 members are here
  • transducers
  • 4-20
  • plc_control
Related

Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?

coolbox
coolbox over 11 years ago

Hi there,

 

4-20 ma is standard for data acquisition from sensors in industrial environment.There are are many techniques like PWM and DAC for 4-20 ma current generation.But still i want to hear from automation experts for options about generating 4-20 ma.Is any micro controller which can directly output 4-20ma?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem +1
    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    I've never used this sort of current loop myself, so this is only an attempt to be helpful -- YMMV.

     

    There's an article about Current Loop at Wikipedia that might have useful background and links: http://en.wikipedia.org/wiki/Current_loop.

     

    The Cypress PSoCs have "high drive" outputs, but I don't know if they go as high as 20 mA.  I suspect you'll need to make a current source using an external transistor or op amp: http://en.wikipedia.org/wiki/Current_source#Simple_transistor_current_sources

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem

    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate quite a range of wiring resistance in the loop without affecting the readings (Within the limits of the MAX Volts of the loop source)

     

    I worked with 4-20mA for years with British Gas for instrumentation of all sorts of sensing (Pressure, Flow, Temperature etc)

     

    Ahh the memories image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem

    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate quite a range of wiring resistance in the loop without affecting the readings (Within the limits of the MAX Volts of the loop source)

     

    I worked with 4-20mA for years with British Gas for instrumentation of all sorts of sensing (Pressure, Flow, Temperature etc)

     

    Ahh the memories image