Robotics
  • Technologies
  • More
Robotics
Forum ADM660 issue on startup
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 76 subscribers
  • Views 1447 views
  • Users 0 members are here
  • adm660
Related

ADM660 issue on startup

femtotech
femtotech over 11 years ago

Hi!

In the schematic attached there is the power section of my board. On the left there is +12VDC, IC1 provides the +3.3V for MCU. IC2 provides about 5.5V and IC3 generates the negative rail (-5.5V).

It works fine, but there is an issue... if the input voltage rises too slow it seems the ADM660 doesn't start to oscillate (the output is 0V) and sinks a lot of current (over 300 mA).

I mean, if I enable the output from a bench power supply, it's very likely it doesn't work. Instead if I plug-in the connector with the bench power supply already enabled it always works.

 

The Vee is connected only to a low-power op-amp (few mA) but I tried to change this with several models and nothing changes, so I assume the problem is just related to the ADM660.

 

Do you see something wrong in my schematic?

I could put a zener diode in series with the input, in order to increase the lowest voltage to feed the regulators... but I would like to understand where is my fault!

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi Marco,

     

    I've used this device before, but in the voltage doubler mode. I didn't observe any issue with it, but I had the LV pin (pin 6) connected to GND. I think it is worth trying this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • femtotech
    0 femtotech over 11 years ago in reply to shabaz

    I've tried right now and there are no changes in the behavior.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to femtotech

    Was this on a device that has drawn 300mA previously? It may have a permanent fault : (

    Unfortunately I've not seen this issue with the ADM660 in the voltage doubler mode. But since the LV pin was specifically mentioned

    should be connected to GND for low voltage operation (and _could_ be connected to GND otherwise) I had connected mine.

    You might want to ask on the AD forum too, in case someone can recognise this issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • femtotech
    0 femtotech over 11 years ago in reply to shabaz

    The behavior has not changed since the first power on. Of course it could be a defect of this specific unit, but at the moment I don't have a replacement. I'm going to ask also on the AD forum, as you suggested.

    Thank you very miuch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • femtotech
    0 femtotech over 11 years ago in reply to shabaz

    The behavior has not changed since the first power on. Of course it could be a defect of this specific unit, but at the moment I don't have a replacement. I'm going to ask also on the AD forum, as you suggested.

    Thank you very miuch