Products
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
Robotics
  • Technologies
  • More
Robotics
Forum Testing rear window defroster grid
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 1 answer
  • Subscribers 78 subscribers
  • Views 8315 views
  • Users 0 members are here
  • plc
  • testing
  • sensors
  • automation
Related

Testing rear window defroster grid

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I would like to develop a testing method to detect window defroster grid failures. Rear windows has 12 heating wires painted to the glass and cca. 2% are faulty pieces.

I tried to measure the resistance, current and voltage drop of good parts and compare results with those where was at least 1 broken wire, but the difference was smaller than the tolerance specified by the supplier. (Other problem is that the resistance is greatly depending on the temperature)

Now we are testing visually with a thermo foil but it takes more time and sometimes the operator mistakes or can forget to correctly check thermo foil. It is also very important to not hurt parts during the testing process, so best option would be contactless testing if possible... image

I'am thinking about to make a tool with 12 sensors, 1 sensor to every each heating wire to sense a flowing current in a wire. But I'am not sure that there is any sensor avaible in the market for such a purpose. Finally PLC have to check the outputs of every sensors, if all the 12 wires are good (current is flowing through them) gives visual signal or in case of failure sound alarm or red light flashing.

 

Here is the specification of rear window defroster:

Power: 167,37W ±10%
Current: 12,87A ±1A
Resistance: 1,0 Ohm -10%/+20%
Wire thickness: 0,48mm
In the attachment you can find technical drawing of the window.

Any ideas and suggestions are welcome.

Best regards,

Ate

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    IF money is not too much of an issue then a thermal camera would instantly show you the broken wire this may set you back 1000$ but would return that pretty quickly in time saved
  • jw0752
    jw0752 over 11 years ago +2 suggested
    Hi Iansm, I had some time this evening and decided to breadboard and test the one Hall Effect device I have in my build stock: SS49E Here is a link to the Newark listing: http://www.newark.com/webapp/wcs…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    Sticking with my suggestion of Hall effect sensors and Johns excelent testing of such, but thinking about the low signal to noise ratio, one option would be to significantly increase the current... AKA…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Lansm

    I have a heat sensor that I use in the lab that has a very low mass thermistor. I suspect that it could be moved across a wire to detect if any heat was being produced. None of our solutions so far will tell you where in the wire there is a break, just that there is a break somewhere. I suspect that some sort of a capacitive sensor dragged along a broken wire might be able to detect the break where there is a potential gradient across the break but I have no empirical experience with this.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to jw0752

    Actually my post to use a thermal camera / imager would show you image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I actually like your idea the best and if it is a partial break in the heating element your thermal scan would show the high resistance area as a bright point. However if there is a total break in the wire there will be no current and no heat and the actual point of the break will not show in the IR camera.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I actually like your idea the best and if it is a partial break in the heating element your thermal scan would show the high resistance area as a bright point. However if there is a total break in the wire there will be no current and no heat and the actual point of the break will not show in the IR camera.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to jw0752

    Very true, you will not be able to see where the break is for a particular element on the window but it will easily show it is broken so from a QA perspective it will be very efficient to weed out the broken ones

     

    if further diagnosis is required on a broken one then that is alo more complex and the camera wil not help

     

    measuring the current, temperature etc will also not help (All of the above examples), now a visual inspection would also be quicker because you atleast know the broken element

     

    down side with the inaging camera is it is not automated (Could be but would be expensive), if as mentioned in the post an automated process is required then one solution may be to use a hall effect sensor and measure the magnetic field created on each element when current flows, this is contactless and can easily flow to a PLC for taking readings, small coils may also be an option, of course this will require a little more circuitry but totally possible

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Thank you all for your kind support and creative ideas.

    I would like to try to use analoge hall effect sensors because this seems the fastest method and could be easily automated and evaluated with plc. Could you recommend any appropriate sensor, small and sensitive enough? You can see the tool used for window checking and cleaning. I have 4cm gap between the window and the tool if I place window into that. Would it be better to use higher voltage?

     

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to e14 Contributor

    Hi Iansm,

    The sensors will be most effective if they are as close as possible to the wires carrying current. Perhaps they can be put on flexible fingers. The intensity of the magnetic field you are trying to sense will decrease with the square of the distance from the wire. In other words if you double the distance between the sensor and the wire you would have to increase the current 4 fold to compensate. From your specifications it looks like each wire is designed to carry 1 amp. I do not have the experience necessary to recommend a specific Hall Effect sensor but perhaps you can get a couple and experiment to see how close you have to get to obtain reliable readings.

    John