Products
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
Robotics
  • Technologies
  • More
Robotics
Forum Testing rear window defroster grid
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 1 answer
  • Subscribers 78 subscribers
  • Views 8327 views
  • Users 0 members are here
  • plc
  • testing
  • sensors
  • automation
Related

Testing rear window defroster grid

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I would like to develop a testing method to detect window defroster grid failures. Rear windows has 12 heating wires painted to the glass and cca. 2% are faulty pieces.

I tried to measure the resistance, current and voltage drop of good parts and compare results with those where was at least 1 broken wire, but the difference was smaller than the tolerance specified by the supplier. (Other problem is that the resistance is greatly depending on the temperature)

Now we are testing visually with a thermo foil but it takes more time and sometimes the operator mistakes or can forget to correctly check thermo foil. It is also very important to not hurt parts during the testing process, so best option would be contactless testing if possible... image

I'am thinking about to make a tool with 12 sensors, 1 sensor to every each heating wire to sense a flowing current in a wire. But I'am not sure that there is any sensor avaible in the market for such a purpose. Finally PLC have to check the outputs of every sensors, if all the 12 wires are good (current is flowing through them) gives visual signal or in case of failure sound alarm or red light flashing.

 

Here is the specification of rear window defroster:

Power: 167,37W ±10%
Current: 12,87A ±1A
Resistance: 1,0 Ohm -10%/+20%
Wire thickness: 0,48mm
In the attachment you can find technical drawing of the window.

Any ideas and suggestions are welcome.

Best regards,

Ate

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    IF money is not too much of an issue then a thermal camera would instantly show you the broken wire this may set you back 1000$ but would return that pretty quickly in time saved
  • jw0752
    jw0752 over 11 years ago +2 suggested
    Hi Iansm, I had some time this evening and decided to breadboard and test the one Hall Effect device I have in my build stock: SS49E Here is a link to the Newark listing: http://www.newark.com/webapp/wcs…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    Sticking with my suggestion of Hall effect sensors and Johns excelent testing of such, but thinking about the low signal to noise ratio, one option would be to significantly increase the current... AKA…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Sticking with my suggestion of Hall effect sensors and Johns excelent testing of such, but thinking about the low signal to noise ratio, one option would be to significantly increase the current... AKA use a pulse rather than a continious current of say 100Amps

     

    LESS HEATING

    MORE MAGNETIC STRENGTH

    EASY TO DO

     

    so have a capacitor charged upto 60V say, or simply have a 60V psu but the cap ensures there will be no long term high current flowing. Use a fet/thyristor to quickly discharge across the heater and at that point all the HALL sensors should have a massivly bigger field to detect, this could all be controlled via the PLC but the output of the hall sensors may need to be latched if the pulse is too quick for the PLC to capture (It may have edge detection inputs as an option ?? )

     

    I can not think why this would not work, it should do no harm to the heater / screen and is quick and simple and should resolve the issue with the small signal john has been seeing

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    I took your suggestion and set up the test using the same Hall Effect sensor but I charged a 1000 uF capacitor to 60 volts and discharged it into a 10 ohm load in series with a wire run across the sensor's sweet spot. I also had the scope set to capture the 60 volt pulse on channel one as well as the pulse from the sensor output on channel two. I read the output of the sensor through a 100 nF cap to eliminate the DC bias. Here is the setup on the bench.

     

    image

     

    And

     

    image

     

    Here is a photo of the waveform obtained. Sorry the trigger info got left in the shot. I will also include bitmaps from the scope of dots and vectors.

     

          imageimageimage

     

    As you can see our 60 volt pulse, generating approximately 6 amps peak, caused a delta output of about 18 mA from the sensor. This is a great improvement on the 4 mVolts we were seeing with a static current flowing. I intentionally limited the current in my test to 6 amps which I estimated was about 6 times the normal current in each of the window wires. Iansm could increase this but at some point the test may cause failures if any of the wires have a weak spot.

     

    If one were going to pursue this line of testing it seems that Robert Peter Oakes has us headed in the right direction.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to jw0752

    That is one VERY large 1000uF cap.!

     

    Well done it seems that this approach may be a solution.

     

    Out of interest do you think it could be detected in a coil, which may give a wider area and increased sensitivity.

     

    Robert Peter Oakes

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 11 years ago in reply to jw0752

    That is one VERY large 1000uF cap.!

     

    Well done it seems that this approach may be a solution.

     

    Out of interest do you think it could be detected in a coil, which may give a wider area and increased sensitivity.

     

    Robert Peter Oakes

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to mcb1

    Hi Mark,

    I needed a cap with a capability to handle 60 volts and all I had was one rated at 400 VDC. image  The individual wires that Iansm wants to measure are all embedded in glass so getting any type of coil or inductive loop around them is out. Let me know if I misunderstood your suggestion.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to jw0752

    I think a small bobbin inductor may do the trick with the surface with writing close to the wire ??