Products
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
Robotics
  • Technologies
  • More
Robotics
Forum Testing rear window defroster grid
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 1 answer
  • Subscribers 78 subscribers
  • Views 8319 views
  • Users 0 members are here
  • plc
  • testing
  • sensors
  • automation
Related

Testing rear window defroster grid

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I would like to develop a testing method to detect window defroster grid failures. Rear windows has 12 heating wires painted to the glass and cca. 2% are faulty pieces.

I tried to measure the resistance, current and voltage drop of good parts and compare results with those where was at least 1 broken wire, but the difference was smaller than the tolerance specified by the supplier. (Other problem is that the resistance is greatly depending on the temperature)

Now we are testing visually with a thermo foil but it takes more time and sometimes the operator mistakes or can forget to correctly check thermo foil. It is also very important to not hurt parts during the testing process, so best option would be contactless testing if possible... image

I'am thinking about to make a tool with 12 sensors, 1 sensor to every each heating wire to sense a flowing current in a wire. But I'am not sure that there is any sensor avaible in the market for such a purpose. Finally PLC have to check the outputs of every sensors, if all the 12 wires are good (current is flowing through them) gives visual signal or in case of failure sound alarm or red light flashing.

 

Here is the specification of rear window defroster:

Power: 167,37W ±10%
Current: 12,87A ±1A
Resistance: 1,0 Ohm -10%/+20%
Wire thickness: 0,48mm
In the attachment you can find technical drawing of the window.

Any ideas and suggestions are welcome.

Best regards,

Ate

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    IF money is not too much of an issue then a thermal camera would instantly show you the broken wire this may set you back 1000$ but would return that pretty quickly in time saved
  • jw0752
    jw0752 over 11 years ago +2 suggested
    Hi Iansm, I had some time this evening and decided to breadboard and test the one Hall Effect device I have in my build stock: SS49E Here is a link to the Newark listing: http://www.newark.com/webapp/wcs…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    Sticking with my suggestion of Hall effect sensors and Johns excelent testing of such, but thinking about the low signal to noise ratio, one option would be to significantly increase the current... AKA…
Parents
  • shabaz
    0 shabaz over 11 years ago

    Provided you can disconnect it, I'd be tempted to just make an oscillator.

    With a 1nF cap in series, the resonant freq may be around 1MHz, and a single wire break may change the frequency (i.e. increase it) by around 5%

    (back of envelope calculations). You'd need to keep any additional wiring short to maximise this change in frequency.

    I've no idea if it is feasible, but could be worth a try.

     

    EDIT: A more modern way could be to try the LDC1000 - there is a pre-built eval board for the LDC1000eval board for the LDC1000 worth a try I suspect.

    Your window defroster is likely just in the right ballpark for the LDC1000. Snap off the coil part of the LDC1000 eval board, and attach the remainder

    to your defroster, with approx 100pF cap in series.

    Note: I've not used the LDC1000, so I don't know if it is appropriate. But it looks ideal to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Provided you can disconnect it, I'd be tempted to just make an oscillator.

    With a 1nF cap in series, the resonant freq may be around 1MHz, and a single wire break may change the frequency (i.e. increase it) by around 5%

    (back of envelope calculations). You'd need to keep any additional wiring short to maximise this change in frequency.

    I've no idea if it is feasible, but could be worth a try.

     

    EDIT: A more modern way could be to try the LDC1000 - there is a pre-built eval board for the LDC1000eval board for the LDC1000 worth a try I suspect.

    Your window defroster is likely just in the right ballpark for the LDC1000. Snap off the coil part of the LDC1000 eval board, and attach the remainder

    to your defroster, with approx 100pF cap in series.

    Note: I've not used the LDC1000, so I don't know if it is appropriate. But it looks ideal to me.