Robotics
  • Technologies
  • More
Robotics
Forum Quick question: D.C. Power and motor controllers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 3 answers
  • Subscribers 77 subscribers
  • Views 890 views
  • Users 0 members are here
Related

Quick question: D.C. Power and motor controllers

braedan
braedan over 9 years ago

Hello element 14 community! Thank you for taking the time to view my question.

 

So I have a legit arduino mega controlling 3, dual motor drivers. Specifically two sabertooth2x12's and one L298N circuit board. So far I have wired the saberteeth in a pwm control mode, so one wire per motor and a ground wire. That's two ground pins taken on the mega, which is no big deal but my L298N also needs a ground pin. I was wondering if since all three motor drivers are running of the same battery and two of the three driver are grounded, that if the last motor driver (L298N) actually needs to connected to another ground pin on the arduino. Could the circuit still work if only one driver was connected to arduino? Even more like my current setup -- two out of three drivers.

 

Thank you!!!

 

P.S - the arduino is going to be running off a separate power source

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +3 suggested
    All the grounds should be going to the same point. The best place for this is on the power supply. Not the arduino If the motor power supply is seperate to the arduino power then tie the two grounds together…
  • braedan
    braedan over 9 years ago in reply to Robert Peter Oakes +1 suggested
    Thanks peteroaks. I get what your trying to say, but I am not trying to run the ground directly to Arduino -- just the ground provided by the motor controllers. sorry for any confusion; heres an sketch…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to braedan +1 suggested
    So I would suggest one ground to each sabertooth as you clearly show, and one ground to the L298N driver, these are all signal grounds rather than "Power Grounds". If you rely on the ground via the saber…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    All the grounds should be going to the same point. The best place for this is on the power supply. Not the arduino

     

    If the motor power supply is seperate to the arduino power then tie the two grounds together

     

    What you don't want is all that ground current going through the arduino pins. These should only carry the signal return current that would be measured in the milli amp range only

     

    Hope this answers your question

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • braedan
    0 braedan over 9 years ago in reply to Robert Peter Oakes

    Thanks peteroaks. I get what your trying to say, but I am not trying to run the ground directly to Arduino -- just the ground provided by the motor controllers. sorry for any confusion; heres an sketch to better explain my predicament.

    image

    would the L298N module still work correctly? my thinking is since the is a ground connection to Arduino and the foreign power source from the other motor drivers there's no need for another one right? one or all three? thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to braedan

    So I would suggest one ground to each sabertooth as you clearly show, and one ground to the L298N driver, these are all signal grounds rather than "Power Grounds". If you rely on the ground via the saber tooth conrols then you may get too much nooise and even risk damage to the arduino.

     

    As you have separate power to the arduino and the motor drivers, this is an ok approach and recommended.

     

    Regards

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to braedan

    So I would suggest one ground to each sabertooth as you clearly show, and one ground to the L298N driver, these are all signal grounds rather than "Power Grounds". If you rely on the ground via the saber tooth conrols then you may get too much nooise and even risk damage to the arduino.

     

    As you have separate power to the arduino and the motor drivers, this is an ok approach and recommended.

     

    Regards

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer