Robotics
  • Technologies
  • More
Robotics
Forum Any Matlab Help or Professionals? #HELPaNOOB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 8 answers
  • Subscribers 78 subscribers
  • Views 2862 views
  • Users 0 members are here
Related

Any Matlab Help or Professionals? #HELPaNOOB

the_future
the_future over 7 years ago

please helppp!!!!

 

just brought one of many new engineering books and the one I started is on Matlab

for robotics and the toolbox but need help with the questions.

 

 

here are the questions

 

This will be based on a series of experiments with the Lynxmotion1 robot arm.

 

  1. Derive a DH representation of forward kinematics for the Lynxmotion arm.

 

 

  1. Analyse the workspace of the robot’s end-effector when each preceding joint moves through its range of motion and plot its 2D views.

 

 

  1. Derive the inverse kinematics for the Lynxmotion arm using the Robotic Toolbox in MATLAB. Test a IK model in 3 different Cartesian positions and demonstrate the accuracy of your model (include necessary comparisons). Create the appropriate plots.

 

 

  1. Plan a task* in MATLAB with at least 5 positions, plot the robot and show an investingation. This process should give you 5 sets of Cartesian coordinates (x,y,z) and angles yaw, pitch, roll specifying the end-effector position and orientation in 3D space (Task: is to pick up a small ball and put it in a cup).

 

 

  1. Solve the Inverse Kinematics for these positions in 3D space and obtain sets of Joint Parameters. Create an appropriate plot/animation in MATLAB (use Robotic Toolbox) for the motion of the robot. MOVE THE ROBOT between the points (film the motion of the robot and provide the video).

 

 

  1. Use a set of Lynxmotion arm joint values to create a free motion trajectory between the points

 

 

  1. Implement a velocity profile with at least 3 different velocities (e.g. start, intermediate and end velocities) (MATLAB only)

 

 

  1. Do a full FK Lynxmotion arm and explain how you can derive the closed-form IK model
  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago +8 suggested
    Seeing your other two posts today Circuit Helpp!! and Circuit Help I'm going to be a bit blunt (almost rude) in my reply. This post and your other two do not give the E14 community any idea of where you…
  • Gough Lui
    Gough Lui over 7 years ago in reply to 14rhb +3 suggested
    Seems like someone just wanted help with their homework ... - Gough
  • 14rhb
    14rhb over 7 years ago in reply to the_future +3 suggested
    Thank you for explaining the background to your questions and honesty about why you are asking, it helps a lot. This is an interesting topic and something I know little about, but I am interested to read…
Parents
  • 14rhb
    0 14rhb over 7 years ago

    Seeing your other two posts today Circuit Helpp!!  and Circuit Help  I'm going to be a bit blunt (almost rude) in my reply. This post and your other two do not give the E14 community any idea of where you have got to before getting stuck, they just state you have a problem and want help sorting it, which is fine; but you have to put effort in as well. I appreciate we all get stuck somewhere from initial idea to finished project but usually we will have a good attempt at solving the task by doing some reading of the material before posting a request for help. Your post above is just a series of complex questions that I assume you want someone to do all the hardwork for you. This post relates to Matlab - so how much Matlab programming have you done? If the answer is none then I would suggest reading up on the basics via something like this https://www.tutorialspoint.com/matlab/ or https://learntocode.mathworks.com/

     

    For instance, I tried to learn to program the STM32 microcontroller and had real difficulties in the compiler basics, I tried out several approaches over a couple of days. Read some more. Asked simple questions in forums to edge me along. Gradually and from several sources I was able to progress, learnt a lot along the way and made some new online 'buddies' in the various forums.

     

    In your above post add some detail to explain what part of each question you don't understand.

     

    Rod

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to 14rhb

    All of that +

     

    @ Future Orlando,

     

    Do you have access to the robot arm and MATLAB with the Robotics toolbox ?

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the_future
    0 the_future over 7 years ago in reply to michaelkellett

    yes just brought everything but the book I have goes really deep into the maths side

    which I don't understand as I am just coming into the engineering world image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • the_future
    0 the_future over 7 years ago in reply to michaelkellett

    yes just brought everything but the book I have goes really deep into the maths side

    which I don't understand as I am just coming into the engineering world image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer