Robotics
  • Technologies
  • More
Robotics
Forum ESD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 6 answers
  • Subscribers 78 subscribers
  • Views 3960 views
  • Users 0 members are here
Related

ESD

rajkiransingh
rajkiransingh over 6 years ago

Hi ,

 

I have developed a robotic modle in that I am facing couple of problems one is with ESD.

The robotic car consists of 4 drive wheels. When it moves for some distance after that when I touch that robot it gives shock. I think it should be electrostatic.

Can you help how to over come this.

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 6 years ago +3 suggested
    If it is just electrostatic build up, just run a ground wire off the vehicle so that it can discharge the surface when it stops. Some wire and a metal washer or nut on the end would do it. I would carefully…
  • shabaz
    shabaz over 6 years ago +2 suggested
    Same solution as a vehicle ground strap surely? You've probably got some friction going on.. rubber tyres or plastic shafts or gears.
  • jw0752
    jw0752 over 6 years ago +2 suggested
    If you can't find a way to install a ground you could try an air discharge. You do this by having a lot of very sharp points. If you have some very fine stranded wire you can strip off the insulation and…
  • dougw
    0 dougw over 5 years ago in reply to rajkiransingh

    You could also try using cotton cloth for the mop as it should have less triboelectric charge buildup than synthetic materials.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to rajkiransingh

    You can drag a ground strap as suggested above.

    It may be possible to design an active system based on a sense electrode and a power electrode, both of which need to be in contact with the ground.

    If you look up cathodic protection systems, they perform a similar function, but beware that the ones designed for boats generally work, however the systems designed for cars generally are not designed properly and won't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<