Robotics
  • Technologies
  • More
Robotics
Forum Degree of climbing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 75 subscribers
  • Views 1504 views
  • Users 0 members are here
Related

Degree of climbing

rajkiransingh
rajkiransingh over 6 years ago

Hi

Am designing a bot , basically which will be moving on the smooth surface (as glass).

The total weight of the bot is around 7kg to 9 kg.

Am i wana use 2 motors.

Climbing angle 0 to 40 degree

Please let me know about which type of motor is should use, what should be the torque, speed etc.,

 

Please guide me if you have got better solutions

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +4 suggested
    At 40 degrees it takes about 5.8 kg to lift a 9 kg bot, which is 57 N. To calculate the torque, multiply by the radius of your drive wheel or drive gear. Add 10% to 20% for friction losses in your drive…
  • jw0752
    jw0752 over 6 years ago +2 suggested
    You will also have to build so that your robot's center of gravity stays within the wheel base at the angle of the incline. John
  • dougw
    0 dougw over 6 years ago

    At 40 degrees it takes about 5.8 kg to lift a 9 kg bot, which is 57 N.

    To calculate the torque, multiply by the radius of your drive wheel or drive gear.

    Add 10% to 20% for friction losses in your drive train.

    Divide by the number of drive motors.

    Add a safety factor.

    You can calculate speed by how fast the circumference of your drive wheel is moving at this torque.

    Note, you will need a pretty good coefficient of friction on your drive wheel to avoid slipping  on a 40 degree slope.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago

    You will also have to build so that your robot's center of gravity stays within the wheel base at the angle of the incline.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer