Robotics
  • Technologies
  • More
Robotics
Forum RTC (Real Time clock) Cypress oscillator fails (oscf flag = 1), what happens ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 76 subscribers
  • Views 1730 views
  • Users 0 members are here
  • "real
  • clock"
  • rtc
  • time
  • cypress
Related

RTC (Real Time clock) Cypress oscillator fails (oscf flag = 1), what happens ?

mmtsuchi
mmtsuchi over 17 years ago

Hi,

 

On a custom bord, I have a RTC Cypress CY14B101k wich is a nvRAM, with Real Time Clock Calendar, Alarm Clock and Watchdog.

This board uses a superCapacity (not battery) for this "RTC".

 

When the board is OFF, RTC is running quite well : the time seems correct.

 

The problem is when the board is ON, the RTC seems stopped and OSCF (Oscillator Failure) flag is set to 1.

My question is : What are the reasons that causes oscillator stop ?

 

I don't use Watchdog, alarm, interrupt.

Writing a 0 to OSCEN_n causes OSCF=0 (good) but 6 seconds later OSCF=1 and the time is not running.

 

Best regards,

  • Sign in to reply
  • Cancel
Parents
  • Oliver
    0 Oliver over 17 years ago
    Hi:
     
    “RTC seems stopped and OSCF (Oscillator Failure) flag is set to 1” does not mean that the oscillator stopped working. You should check either it works or not.
     
    Following is the description in CY14B101K datasheet:
     
    “When the device is powered on (VCC goes above VSWITCH), the OSCEN bit is checked for “enabled” status. If the OSCEN bit is enabled and the oscillator is not active within the first 5 ms, the OSCF bit is set to “1”. The system must check for this condition and then write ‘0’ to clear the flag. Note that in addition to setting the OSCF flag bit, the time registers are reset to the “Base Time” (see “Setting the Clock” on page 7), which is the value last written to the time keeping registers. The Control or Calibration registers and the OSCEN bit are not affected by the “oscillator failed” condition.”
    The OSCF is Set to 1 on power up if the oscillator is enabled and not running in the first 5 ms of operation. This indicates that RTC backup power failed and clock value is no longer valid. The user must reset this bit to 0 to clear this condition (Flag). The chip does not clear this flag.
     
    It seems that the clock value is no longer valid, not “RTC seems stopped”, Maybe.
     
    Best wishes,
    Oliver zhang
    Attachments:
    imageCY14B101K1.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mmtsuchi
    0 mmtsuchi over 17 years ago in reply to Oliver

    Thanks for the answer.

     

    I "scoped" the quartz signals. I may introduce impedance with the oscilloscope.

     

    When the RTC chip is on CAPacitor, I can see sinusoïdal waveform with an offset. VX1= 0.4Vac + 0.6Vdc

     

    When the RTC chip is not sollicited (Address bus and data bus not changed during 10  seconds), I can see high sinusoïdal waveform VX1= 1.4Vac + 0.7Vdc

     

    This RTC chip shares its address bus and data bus with SRAM and FLash.

    Tests of address bus and data bus (verify if one is "stuck") are OK.

     

    On a Application Note form Cypress, it is reported that undershoot may stop Oscillator. I put Schottky diode on critical signals to limit undershoot.

    But no changes.

     

    It is like Oscillations are "pumped" to 0V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mmtsuchi
    0 mmtsuchi over 17 years ago in reply to Oliver

    Thanks for the answer.

     

    I "scoped" the quartz signals. I may introduce impedance with the oscilloscope.

     

    When the RTC chip is on CAPacitor, I can see sinusoïdal waveform with an offset. VX1= 0.4Vac + 0.6Vdc

     

    When the RTC chip is not sollicited (Address bus and data bus not changed during 10  seconds), I can see high sinusoïdal waveform VX1= 1.4Vac + 0.7Vdc

     

    This RTC chip shares its address bus and data bus with SRAM and FLash.

    Tests of address bus and data bus (verify if one is "stuck") are OK.

     

    On a Application Note form Cypress, it is reported that undershoot may stop Oscillator. I put Schottky diode on critical signals to limit undershoot.

    But no changes.

     

    It is like Oscillations are "pumped" to 0V.