Robotics
  • Technologies
  • More
Robotics
Forum Displacement Sensor for automation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 79 subscribers
  • Views 1022 views
  • Users 0 members are here
  • research
  • photonics
  • university
  • automation
Related

Displacement Sensor for automation

benjamin_taylor
benjamin_taylor over 13 years ago

Greetings element 14 community,

 

I work as a graduate student at the university of toronto. I am working on making an autoamted photonic chip testing station. I currently am solving the problem of aliging a fiber array to an array of grating couplers. One major issue with this is the possability of landing the fiber tips onto the chip (bad news bears). So to alliviate this problem we are looking into some sort of "height" sensor to detect the distance between the fiber tips (built into a fiber array) and the top of the chip.

 

I have looked into many sensor types but can not find one that meets all of my needs which are:

 

  • Sub micron accuracy... The ideal coupling distance from fiber tip to coupler is 5-10um. So we will need a measuremnt of for example 5.3um needing 0.X accuracy
  • Range of 10um ie, the sensor will work form 0um from chip to 10um from chip (or larger, this is a minimum requirement)
  • The chips we make on average are 4x6mm and made of silicon materials. (passive structures are the most common) so the sensor must be able to detct said materials. Thickness is variable depending on what structurs are layed out. but will always be <1mm
  • Spot size small enough to detect features on top of the cip, waveguides etc.

 

Some things I have looked into so far are the E2C - EDA series capacative sensors by OMRON. However as far as I can tell this sensor can not detect objects that are the size of my chip.

 

I have also considered using an optical sensor but so far the sizes of the probe have been a problem. In order for the system to work I need the probe to sit on top of the Fiber Array which is a rectangle of about 13mm long and has a width depending on how many fibers you include ~ 4-6mm.

 

My question is thus:

 

"Can you suggest any sensor that would be able to meet all of my needs?"

 

Thank you,

 

Benjamin Taylor (University of Toronto)

  • Sign in to reply
  • Cancel
  • Catwell
    0 Catwell over 13 years ago

    Ben,

     

    Do you want the suggested device be completely automated for PCB inspection?

    Or would a manual, optical, viewer be ok?

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • benjamin_taylor
    0 benjamin_taylor over 13 years ago in reply to Catwell

    I was hoping automated. In that I can access the height measurement on a

    computer and use the value when coding my automated testing set-up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Benjamin Taylor,

     

    I would personally use a Vision System like a Cognex In-Sight, because you can program them the way you want.

    They have autofocus, fast image capture, integrated lighting and lens with powerful vision tools.

    With their software you can configure it to control lenght and much more.

    You can get more information here: In-Sight 7000 Series.

     

    I hope that this information will help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Keyance CV5002 Series Cameras are also very good based on the programming capabilities.  Super High Speed Multi-Camera Machine vision systems such as these can capture multiple, key characteristics and are extremely accurate.    Depending on how versed you are on camera specific identification functions, you may find that IV Navigator (Keyence software) is a very user friendly interface particularly during set-up.  Good luck. Either way, I believe that a vision system is the correct choice.  When it boils down to price, you will find yourself limited to many otherwise available options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 12 years ago

    Your stuff probably isn't all that conductive, which is too bad. Maybe we could use a quantum tunneling effect like atomic force microscopy to detect proximity.

    Perhaps you could modify this technique to do your sensing:

     

    Ultrasonic force microscopy - Wikipedia, the free encyclopedia