Robotics
  • Technologies
  • More
Robotics
Forum Industry isolated communication
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 79 subscribers
  • Views 2621 views
  • Users 0 members are here
  • industry
  • communication
Related

Industry isolated communication

ltomi91
ltomi91 over 11 years ago

Dear Everybody!

 

I search the best solution for the following problem.

I want to establish isolated communication between two devices. 2x 8 input and 8 output should be connected (one-way). First think the optocoupler, but it requires a lot of wires, and these devices are in a noisy, industry environment, so necessary the good interface, e.g. RS485. I was looking for any "target" IC, but could not find it.

I attached a picture from this situation.

 

Thank you in advance (and sorry for my english image ) !

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    and from a non optical approach, TI has some isolated tranceivers for RS485 for a few $$$ each http://www.ti.com/lit/sg/slyt484a/slyt484a.pdf these provide full galvanic isolation upto about 4KV Either…
  • michaelkellett
    michaelkellett over 11 years ago +1
    You haven't really told us enough but if you can get away with RS485 speeds why not use a fibre optic link. Plastic fibre and associated parts are quite cheap and easy to use - you would need one twin…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    What are the two devices, what voltge levels are we dealing with and how far apart are they, as Michael has already stated, more information would be very handy to enable us to help you better
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    and from a non optical approach, TI has some isolated tranceivers for RS485 for a few $$$ each

    http://www.ti.com/lit/sg/slyt484a/slyt484a.pdf

     

    these provide full galvanic isolation upto about 4KV

     

    Either way you still need the Parallel to serial conversion of your data or many isolated traceivers, it is how you get from location A to location B that is the descussion here image

     

    Fiber will add a couple of hundred $$ to the cost or more depending on where you shop and may need ethernet as the connection at each end which is also a viable option btw and ethernet also provides isolation due to its termination transformers at each end of the cable

     

    Ethernet will provice about 1000V of isolation on its own

     

    from a cost, Ethernet and RS485 should be the cheapest, optical more expensive but providing superior isolation if needed

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to Robert Peter Oakes

    Plastic fibre will add far less than $200 to the cost and no way does it need ethernet.

     

    You can connect low cost optical transceivers directly to the UART ports of the micro.

     

    TX HFBR-1522Z (Farnell 1173129 £8.80) - will need a driver chip but it's not expensive

    RX HFBR-2522Z (Farnell 1173132 £8.88)

    The data sheet from Avago is helpful on these parts.

    20metre coil of cable (Rapid Electronics 58-0710 £20.81)

     

    Ethernet (using the usual cables and transformers) is an option but needs much more software and more expensive and complicated micros at each end. There are some TI launchpad thingies with Ethernet built in which might make a simple way to go.

    (BTW Ethernet transformers are supposed to be tested for 1000V breakdown - they are not usually rated for safe use at 1000V and most pcbs are not tracked to provide serious HV isolation. RJ45 connectors may or may not comply with the regulations for creepage distances so any solution with magnetics built into the connectors should be considered as an earth loop avoidance solution but no good for safety isolation (unless you have evidence that they are OK))

     

    100Mbit Ethernet using only basic Ethernet protocol (no IP stack or RTOS) can give very good performance at low cost - any kind of OS and using off the shelf IP software will add a lot of latency and slow things down significantly.

     

     

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to michaelkellett

    I stand corrected, Nice Michael.

     

    I was looking at standard optical units through google and most of them had an ethernet port accociated with them

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to Robert Peter Oakes

    A few years ago I did several very low cost links using the Avago interface bits and plastic fibre but since then it's become much harder to find the twin plastic fibre at a reasonable price.

     

    I've recently worked on a very high performance analogue link (true analogue - no adc or dac, > 100dB S/N) using plastic fibre but the fibre cable was made for the job so out of range of a one off project. We made our own fibre to LED/PD mechanical bits.

     

    Amplicon used to make and sell a very low cost RS232 to fibre converter system but now they only do the Moxa (or similar) ones and they do cost about £100 per end.

     

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Hi Michael,

     

    Very cool to hear about the analogue link. If it is not proprietary information, may I ask, does it use FM? If so, what technique was used for the demodulation - was it quadrature detection?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Hi Michael,

     

    Very cool to hear about the analogue link. If it is not proprietary information, may I ask, does it use FM? If so, what technique was used for the demodulation - was it quadrature detection?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 11 years ago in reply to shabaz

    No - it's baseband linear - done for analogue audiophiles. Two LEDs in push-pull like an audio amp (one does +ve half cycle and other does -ve) two fibres, two receiving photo diodes and recovery amps. Bandwidth about 50kHz, S/N ref about 2% distortion is approx 102dB. I never thought it would work either. It is patented but you can't buy one yet.

     

    I thought there might be industrial applications but haven't thought of one yet.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelkellett

    Hi Michael,

     

    That is very interesting. Thanks for the information!

    If I can think of industrial use-cases, I'll let you know. I'm thinking there are bound to be scenarios where it is too expensive or difficult to process or convert data close to the machine or process - you could remotely do this by transporting sensor signals to a safer or easier environment, e.g. to a control room. Or perhaps automotive scenarios too?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to michaelkellett

    How about remote speakers.

    In our case the workstation is often in the equipment room and the KVM is remoted to the cab (above), but they have an issue with speakers for the audio alerts.

     

    Because these installs generally have VHF/UHF radios, keeping the RF out of the audio is a problem.

     

     

    Mark