Robotics
  • Technologies
  • More
Robotics
Forum Servo trouble
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 52 replies
  • Subscribers 80 subscribers
  • Views 6987 views
  • Users 0 members are here
Related

Servo trouble

royston02
royston02 over 12 years ago

I wanted to know if a servo left without power in stationery mode (without making me want to turn it) lift the weight?

Eg:- A skateboard. I just want to stand on itwithout it moving. the skateboard is the servo. Will the skateboard i.e servo stand or fall? No battery. 

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +2
    If you can live with a normal DC motor and use it with a worm gear, it should "lock" when not powered.
  • mcb1
    mcb1 over 12 years ago in reply to royston02 +1
    Try this .. Open your browse and enter this in a google search "how does a servo work" the first two results give a good breakdown of how it works. Mark
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago +1
    Note there are many different systems that fall under the name of SERVO. The one you linked in may be geared but not like the one shown above. A typical Remote control plane/Car/Boat servo is based on…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago

    If a servo is  not powered it will not resist rotational forces applied to it. So in your words it will fail

     

    there may be some models of servos with locking mechanism but I am not aware of them

     

    a motor can also be so some what braked by shorting it's winding which will cause it to self lock

     

    this could be done with a relay, great care will be needed to not apply power while the relay is closed of course

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    Peter Oakes wrote:

    a motor can also be so some what braked by shorting it's winding which will cause it to self lock

    how to do it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to royston02

    if yo take a simple motor, a small one out of a toy or something

     

    with nothing connected to the motor power pins, try turning the motor, it should move relatively easily

     

    now put a short across the power pins of the motor (No power or anything, just a short), with the short in place, not try to turn the motor

     

    with the short it should be far more difficult or even impossible without significant force to move it, this is because the motor is generating a reverse EMF that ends up opposing the direction of rotation.

     

    this happens with pretty much any motor that has a magnet and coil arrangement

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 12 years ago in reply to royston02

    if yo take a simple motor, a small one out of a toy or something

     

    with nothing connected to the motor power pins, try turning the motor, it should move relatively easily

     

    now put a short across the power pins of the motor (No power or anything, just a short), with the short in place, not try to turn the motor

     

    with the short it should be far more difficult or even impossible without significant force to move it, this is because the motor is generating a reverse EMF that ends up opposing the direction of rotation.

     

    this happens with pretty much any motor that has a magnet and coil arrangement

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • royston02
    0 royston02 over 12 years ago in reply to Robert Peter Oakes

    Peter,

    how would I know which type of motor is inside. Plus how to do it?

    Wong,

    I'm using a servo built, don't want to break the servo. Even if I onpen to attach a worm gear, not sure out to do it and gear ratio. I want one with the exact torque as this one(If hand build)

    -Radio Control Planes, Helicopters, Cars, Boats, FPV and Quadcopters - Hobbyking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to royston02

    There are many worm gear actuators that produce torque in excess of 500 kg-cm.

    There are several modules that will convert standard DC motors into RC servo motors. such as this (RC Power Servo) or (http://www.robot-r-us.com/motor-controller/pololu-simple-high-power-motor-controller-18v25.html)

    There are lots of DC gearmotors with worm gears that can be converted to servo motors.

    There are many servo systems that outperform RC servos.

    There are many motor controllers that may suit your requirements.

    We need to know range of motion, size, weight, speed and cost requirements as well as torque to make any kind of suitable suggestion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to dougw

    I don't want a controller: just a servo

    size-  40*40(4.7 max0)

    range of motion- stationery i.e. 0

    weight- 78gs{ 100 g max(the lesser the better)}

    speed-useless( because range of motion- stationery i.e. 0)

    cost- 70${80$ max(the lesser the better)}

    torque-40kg{no lesser(38kg min with adjustments)}

    Hope this is helpful

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royston02
    0 royston02 over 12 years ago in reply to royston02

    What about winch servos?

    -Radio Control Planes, Helicopters, Cars, Boats, FPV and Quadcopters - Hobbyking

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 12 years ago in reply to royston02

    I don't quite get why a servo is needed if no motion is needed.

    A fixed bracket could do the job described.

    If you want to apply a variable torque - a servo is probably not the best way.

    Any linear actuator could supply holding "torque" - many can do this without power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 12 years ago in reply to royston02

    Greetings Royston, There's something your not telling us. Is the servo only being used to stop movement or is it being used to control the movement.  For example move the load to a position ans hold it there.

     

    Without knowing what it's being used for it difficult for us to help you design this thing you are building. For some reason you are forced to use servos when other devices may be more efficient.

     

    You have some very good ideas here. Maybe we don't understand your requirements.  A little clarification of what it is your trying to make would be extremely helpful.

     

    -Steve