Robotics
  • Technologies
  • More
Robotics
Forum SAND FLEA!? help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 79 subscribers
  • Views 1313 views
  • Users 0 members are here
  • robotics
Related

SAND FLEA!? help

boa
boa over 11 years ago

hello,

 

i am currently studying computer engineering and for my dynamics class i was asked to make a arduino based project that had to do with dynamics.

basically i want to make this:

https://www.youtube.com/watch?v=6b4ZZQkcNEo

 

image

With the modification that it will calculate based on the angle and the force, how high & long it traveled and with what acceleration & velocity 

It doesn't have to jump as much, it would just have to jump about 2m at most, the thing is that i know how to do the build, wheels, circuits, programming my weak spot is the mechanics that will make this thing

jump. I would really appreciate and helpful ideas/tips/comments/ on how to make this thing jump.

 

Thank you element 14 community

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Darpa probably spent millions of US dollars on that cute jumper! This is a huge task to replicate anything close. You should use rubber bands or a spring with a small motor to wind up the action. Forget…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Carl - Here are some thoughts. Keep the mass to a minimum as each gram of added mass will increase the force that has to be delivered to make it jump. To simplify you might want to consider a one shot mechanism that you can *** like a mouse trap that can be triggered once. The force to make it jump has to be delivered through the center of gravity or you will just spin it. If the force is delivered through the center of gravity at a 45 degree angle to the horizontal you should get the most lateral distance for a give force. Since any force producing mechanism that can be put into such a small device will have a fairly short action distance in which to deliver the force it will have to be done quickly.  Another idea would be a CO2 powered piston controlled by a solenoid that can be triggered by the Arduino. This might give you multiple jumps. I loved the video. This is one of those devices that look simple but are actually very high technology. Sorry I can't help you more. Please let us know what you figure out.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Carl - Here are some thoughts. Keep the mass to a minimum as each gram of added mass will increase the force that has to be delivered to make it jump. To simplify you might want to consider a one shot mechanism that you can *** like a mouse trap that can be triggered once. The force to make it jump has to be delivered through the center of gravity or you will just spin it. If the force is delivered through the center of gravity at a 45 degree angle to the horizontal you should get the most lateral distance for a give force. Since any force producing mechanism that can be put into such a small device will have a fairly short action distance in which to deliver the force it will have to be done quickly.  Another idea would be a CO2 powered piston controlled by a solenoid that can be triggered by the Arduino. This might give you multiple jumps. I loved the video. This is one of those devices that look simple but are actually very high technology. Sorry I can't help you more. Please let us know what you figure out.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer