Robotics
  • Technologies
  • More
Robotics
Forum Tiny Robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 80 subscribers
  • Views 1654 views
  • Users 0 members are here
  • kit
Related

Tiny Robot

Workshopshed
Workshopshed over 10 years ago

Here's the latest little robot kit on the block.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Wink— STEM Education Pet Robot | DIYZER

 

I think the price point of $59 is still a bit high though.

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    Nice to see a product aimed at kids that doesn't lock them into a scratch-like environment for a change.
  • Workshopshed
    Workshopshed over 10 years ago in reply to Robert Peter Oakes +1
    The wink has a microcontroller, sensors and outputs in the form of motors and lights. It can operate without being controlled by a human. Surely that makes it a robot. I've just bought myself a bag of…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Land based drone perhaps, A Robot... Na.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to Robert Peter Oakes

    The wink has a microcontroller, sensors and outputs in the form of motors and lights. It can operate without being controlled by a human. Surely that makes it a robot.

     

    I've just bought myself a bag of little vibration motors, I'm going to see if I can build something similar (without sensors) using an Adafruit Trinket

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Workshopshed

    Andy I am not discussing on the correct categorisation or not. What I point is different, especially respect the target this device pretend to be addressed. Just to make an example, if you gift to a kid a train he can enjoy playing with the train, better if it is a perfect replica 1:50 of a real train with all details. Then if to the same kid you gift a perfect running replica of an underground train and he see just a tube because the train run inside, you are giving him the same thing but very few appeal, despite both the two things are of the same category. In the second case he has a dramatically low perception of all what implies to play with a train. He has a tube ! image

    In the same way like this extreme example the received perception of a "robot" for a kid in my opinion is very low in this case, less than the same he can have with a robot arm or a simply programmable thing that can do also the most stupid action than run (ok, this game can follow a black line).

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Workshopshed

    Andy I am not discussing on the correct categorisation or not. What I point is different, especially respect the target this device pretend to be addressed. Just to make an example, if you gift to a kid a train he can enjoy playing with the train, better if it is a perfect replica 1:50 of a real train with all details. Then if to the same kid you gift a perfect running replica of an underground train and he see just a tube because the train run inside, you are giving him the same thing but very few appeal, despite both the two things are of the same category. In the second case he has a dramatically low perception of all what implies to play with a train. He has a tube ! image

    In the same way like this extreme example the received perception of a "robot" for a kid in my opinion is very low in this case, less than the same he can have with a robot arm or a simply programmable thing that can do also the most stupid action than run (ok, this game can follow a black line).

     

    Enrico