Sensors
  • Technologies
  • More
Sensors
Blog Seeed Xiao ESP32S3 Sense
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 30 Apr 2023 11:25 PM Date Created
  • Views 23799 views
  • Likes 8 likes
  • Comments 6 comments
  • xiao esp32s3 sense
  • Xiao
  • seeed xiao esp32s3
Related
Recommended

Seeed Xiao ESP32S3 Sense

ralphjy
ralphjy
30 Apr 2023

The Seeed Xiao is my favorite small form factor development board.  I have quite a few of the original SAMD21 boards.  They're great for prototyping sensors and the family has expanded to use many of the common MCU types - SAMD21, RP2040, nRF52840, ESP32C3 (RISC-V), and their latest uses an ESP32S3.

I've used ESP32-Cam boards in the past, but I was still surprised by the size and cost of the new Xiao ESP32S3 Sense module.  The base Xiao ESP32S3 board costs $7.49 and the Sense option adds a piggyback board with an OV2640 (1600x1200) camera, digital microphone and SD card for an extra $6.50.  That was something that I couldn't pass up, so I bought one and it just arrived.

XIAO ESP32S3 Sense

image

Here is my unit with a quick case that I printed for it.

image

That's a huge WiFi antenna compared to the one that comes with the Nicla Vision Slight smile.

image

Seeed has a github repo with sample applications for the module - https://github.com/limengdu/SeeedStudio-XIAO-ESP32S3-Sense-camera.

I decided to try out the CameraWebServer example.  They do warn you that if you stream continuously that the module will get very hot (I've had that experience with ESP32-Cams also).  I figured if the PLA case started melting that it would be time to stop...

CameraWebServer.ino

#include "esp_camera.h"
#include <WiFi.h>

#define CAMERA_MODEL_XIAO_ESP32S3 // Has PSRAM

#include "camera_pins.h"

// ===========================
// Enter your WiFi credentials
// ===========================
const char* ssid = "**********";
const char* password = "**********";

void startCameraServer();
void setupLedFlash(int pin);

void setup() {
  Serial.begin(115200);
  while(!Serial);
  Serial.setDebugOutput(true);
  Serial.println();

  camera_config_t config;
  config.ledc_channel = LEDC_CHANNEL_0;
  config.ledc_timer = LEDC_TIMER_0;
  config.pin_d0 = Y2_GPIO_NUM;
  config.pin_d1 = Y3_GPIO_NUM;
  config.pin_d2 = Y4_GPIO_NUM;
  config.pin_d3 = Y5_GPIO_NUM;
  config.pin_d4 = Y6_GPIO_NUM;
  config.pin_d5 = Y7_GPIO_NUM;
  config.pin_d6 = Y8_GPIO_NUM;
  config.pin_d7 = Y9_GPIO_NUM;
  config.pin_xclk = XCLK_GPIO_NUM;
  config.pin_pclk = PCLK_GPIO_NUM;
  config.pin_vsync = VSYNC_GPIO_NUM;
  config.pin_href = HREF_GPIO_NUM;
  config.pin_sscb_sda = SIOD_GPIO_NUM;
  config.pin_sscb_scl = SIOC_GPIO_NUM;
  config.pin_pwdn = PWDN_GPIO_NUM;
  config.pin_reset = RESET_GPIO_NUM;
  config.xclk_freq_hz = 20000000;
  config.frame_size = FRAMESIZE_UXGA;
  config.pixel_format = PIXFORMAT_JPEG; // for streaming
  //config.pixel_format = PIXFORMAT_RGB565; // for face detection/recognition
  config.grab_mode = CAMERA_GRAB_WHEN_EMPTY;
  config.fb_location = CAMERA_FB_IN_PSRAM;
  config.jpeg_quality = 12;
  config.fb_count = 1;
  
  // if PSRAM IC present, init with UXGA resolution and higher JPEG quality
  //                      for larger pre-allocated frame buffer.
  if(config.pixel_format == PIXFORMAT_JPEG){
    if(psramFound()){
      config.jpeg_quality = 10;
      config.fb_count = 2;
      config.grab_mode = CAMERA_GRAB_LATEST;
    } else {
      // Limit the frame size when PSRAM is not available
      config.frame_size = FRAMESIZE_SVGA;
      config.fb_location = CAMERA_FB_IN_DRAM;
    }
  } else {
    // Best option for face detection/recognition
    config.frame_size = FRAMESIZE_240X240;
#if CONFIG_IDF_TARGET_ESP32S3
    config.fb_count = 2;
#endif
  }

  // camera init
  esp_err_t err = esp_camera_init(&config);
  if (err != ESP_OK) {
    Serial.printf("Camera init failed with error 0x%x", err);
    return;
  }

  sensor_t * s = esp_camera_sensor_get();
  // initial sensors are flipped vertically and colors are a bit saturated
  if (s->id.PID == OV3660_PID) {
    s->set_vflip(s, 1); // flip it back
    s->set_brightness(s, 1); // up the brightness just a bit
    s->set_saturation(s, -2); // lower the saturation
  }
  // drop down frame size for higher initial frame rate
  if(config.pixel_format == PIXFORMAT_JPEG){
    s->set_framesize(s, FRAMESIZE_QVGA);
  }

// Setup LED FLash if LED pin is defined in camera_pins.h
#if defined(LED_GPIO_NUM)
  setupLedFlash(LED_GPIO_NUM);
#endif

  WiFi.begin(ssid, password);
  WiFi.setSleep(false);

  while (WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }
  Serial.println("");
  Serial.println("WiFi connected");

  startCameraServer();

  Serial.print("Camera Ready! Use 'http://");
  Serial.print(WiFi.localIP());
  Serial.println("' to connect");
}

void loop() {
  // Do nothing. Everything is done in another task by the web server
  delay(10000);
}

The program brings up a browser interface at the module ip address.

image

It allows you to stream and take stills at the different camera resolutions up to the max 1600x1200, but you can't get great frame rate at the higher resolutions.

It also has Face Detection and Face Recognition capability, but only up to QVGA (320x240) resolution which is on par with other ML models I've used.

Sorry I don't have a better looking subject...

image

A short video showing the max resolution down to face detection.  Just realized that the horizontal is flipped (like doing a selfie).

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I can see lots of possibilities for this module.  Made me think of scottiebabe 's birdhouse Smiley.

  • Sign in to reply
  • scottiebabe
    scottiebabe over 3 years ago

    What a cute little sense hat! The formfactor your project achieved is quite remarkable. That ESP definitely has a boot time at least 1 to 2 orders of magnitude less than a RPI lol

    I recently got the RPI camera module 3 and am trying to put it into a rudimentary handheld formfactor.

     image

    I think taking a picture on a button press is within my software skill level Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<