Sensors
  • Technologies
  • More
Sensors
Sensor Forum Questions about Panasonic Grid-EYE Infrared MEMS Sensor WEBINAR Thu 12/3/15??
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 349 subscribers
  • Views 430 views
  • Users 0 members are here
  • sensing
  • ir_sensor
  • temp_light_sensor
  • sensors
  • thermopile
  • mems
  • iot
  • thermal_imaging
  • arduino
  • sensor
  • gesture_control
Related

Questions about Panasonic Grid-EYE Infrared MEMS Sensor WEBINAR Thu 12/3/15??

anitai
anitai over 10 years ago

Hey,

 

Experts will be available to answer your questions on the new Panasonic Grid-EYE Infrared Array Sensor and Evaluation Kit tomorrow.

 

It can detect multiple people or objects moving in different directions; up, down, left, right and diagonally, including hand movements for gesture control.

 

 

 

Features

 

64 thermopile elements in an 8x8 grid format

 

Possible to detect multiple persons, identify positions and direction of movement

 

Dimensions: 11.6 x 4.3 x 8.0mm (L x H x W)

 

Operating voltage: 3.3V or 5.0V (depends on P/N)

Field of view: 60° (vertical and horizontal

 

 

JOIN WEBINAR & WATCH PRODUCT VIDEO HERE > http://www.element14.com/community/events/4485

 

When and Where

               

  • Start Time:

    12/3/2015 3:00 PM GMT (Europe/London)
  • End Time:

    12/3/2015 4:00 PM GMT (Europe/London)
  • Location:

    WebEx

 

Priced from $65.12 / £47.20 / €64.99 the Grid-EYE Evaluation Kit is available from Farnell element14 in Europe, Newark element14 in North America and element14 in Asia Pacific.

The kit has two modes of operation, the kit can function as a standalone device or it can be connected to an Arduino platform.

image

See you there,

Anita

Attachments:
imagePanasonic-Grid-EYE-Evaluation-Kit-Manual.pdf