Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensing Baby Kicks
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 350 subscribers
  • Views 2610 views
  • Users 0 members are here
  • ip_iot
Related

Sensing Baby Kicks

ipv1
ipv1 over 10 years ago

I have made a belt for sensing when our unborn child kicks from the inside. This is useful for tracking activity and health of the baby. In my current configuration, I am using a piezoelctric sensor strip but there are a few issues.

  1. The strip is small and cannot cover a large surface area.
  2. It will not discriminate between kicks and movement caused by the mother herself.


I was able to condition the signals and send them over BTLE but the sensor is an issue.

Can anyone suggest? Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 10 years ago +3
    Interesting theories. Dough 's solution will need too much tweaking but will be a better one in the long run. Jan's solution has one issue- the cloth worn tightly will be uncomfortable over time. But I…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to ipv1 +3
    In my defence, I'm going to suggest to buy stretching resistive cloth
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps +3
    http://openmaterials.org/materials-101-electrotextiles/ Electrolycra from Mindsets : looks and feels like ordinary lycra but it’s highly conductive. Its conductivity in one direction depends on how tightly…
Parents
  • ipv1
    ipv1 over 10 years ago

    Interesting theories. Dough 's solution will need too much tweaking but will be a better one in the long run.

    Jan's solution has one issue- the cloth worn tightly will be uncomfortable over time.

    But I'm getting good ideas. More inputs please. image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to ipv1

    In my defence, I'm going to suggest to buy stretching resistive cloth image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    http://openmaterials.org/materials-101-electrotextiles/

     

    Electrolycra from Mindsets: looks and feels like ordinary lycra but it’s highly conductive. Its conductivity in one direction depends on how tightly it is stretched – if you pull it the resistance increases and then drops again when stretched even tighter. When cut into a thin strip, the material also warms up when current is passed through it and can thus provide the basis of a heated garment. A 6V battery will cause an appreciable warming effect. Resistivity: 5 ohms per 100mm, increasing to 20 ohms when stretched to 150mm. If the material is turned through 90º and stretched the resistance drops to 2.5 ohms

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Jan Cumps

    http://openmaterials.org/materials-101-electrotextiles/

     

    Electrolycra from Mindsets: looks and feels like ordinary lycra but it’s highly conductive. Its conductivity in one direction depends on how tightly it is stretched – if you pull it the resistance increases and then drops again when stretched even tighter. When cut into a thin strip, the material also warms up when current is passed through it and can thus provide the basis of a heated garment. A 6V battery will cause an appreciable warming effect. Resistivity: 5 ohms per 100mm, increasing to 20 ohms when stretched to 150mm. If the material is turned through 90º and stretched the resistance drops to 2.5 ohms

    • Cancel
    • Vote Up +3 Vote Down