Sensors
  • Technologies
  • More
Sensors
Sensor Forum Magnetic Rotary Position Sensors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 350 subscribers
  • Views 2748 views
  • Users 0 members are here
Related

Magnetic Rotary Position Sensors

Workshopshed
Workshopshed over 13 years ago

I'm hoping to evaluate the AS5048B sensor for a rotary table solution.

 

http://www.ams.com/eng/Products/Magnetic-Position-Sensors/Rotary-Magnetic-Position-Sensors/AS5048B

 

There's a bullet point on the description that reads:

 

"Angle accuracy 0.05°after system linearization and averaging"

 

I understand about averaging but what is mean by system linearization and how would I go about doing that?

 

Has anyone used this model or others in the series? Product LinkProduct Link

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 13 years ago in reply to Workshopshed +1
    Bit more progress on the test rig http://www.workshopshed.com/2013/06/magnetic-sensor-test-rig.html
Parents
  • shabaz
    shabaz over 13 years ago

    The ams.com website is down currently so I couldn't see the datasheet, but that's really impressive if they can achieve this accuracy, and if the resolution is high. Glad you're investigating!!! I wonder if that means people don't need to spend a fortune on optical encoders for some high-accuracy applications. For a tool application, it would be interesting to know if motors/cables nearby or any other magnetic fields affect it. Have you noticed any fluctuations in your measurements?

    EDIT: just saw the Farnell link. That's very low cost! But, I was unsure, the datasheet on the Farnell site said +-0.5 degree accuracy, is this different to the manufacturer site? I guess with gearing and keeping a count of revolutions, that is still pretty good. But then there is the issue of eliminating backlash I guess :-(

    I remember reading some micrometers don't use optical encoders either, but use some accurately spaced parallel PCB tracks, and capacitance. Just as a slight digression,  it doesn't help your use-case directly, but the FRDM-KL25Z boards have a lot of capacitive sensor inputs. I wonder if they can be re-tasked to some measurement purpose. That would be pretty amazing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 13 years ago in reply to shabaz

    The encoders still have their purpose; firstly they go to even higher resolution (2000 pulses per revolution no exception in robotics). Secondly, resolution is not the only concern:

    • Accuracy is not 14-bit, as you have 2.7 bit rms noise. Of course you can average, but that will cost speed
    • Sampling rate is 11kHz, so in very fast rotating axes the bandwith of measurement is impaired; not so with encoders

    Nevertheless, magnetic rotational encoders have a very wide range of applications, and it's cool to measure just by adding a magnet!

    A company that has made a very high accuracy motor driver for us told me that they're primarily using IC's from IC-Haus: http://www.ichaus.de/keyword/Magnetic%20Encoder%20iCs.

    This company is also interesting: http://www.rls.si/en/am512b-9-bit-rotary-magnetic-sensor-chip--15882#ElementMediaList40407

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vsluiter
    vsluiter over 13 years ago in reply to shabaz

    The encoders still have their purpose; firstly they go to even higher resolution (2000 pulses per revolution no exception in robotics). Secondly, resolution is not the only concern:

    • Accuracy is not 14-bit, as you have 2.7 bit rms noise. Of course you can average, but that will cost speed
    • Sampling rate is 11kHz, so in very fast rotating axes the bandwith of measurement is impaired; not so with encoders

    Nevertheless, magnetic rotational encoders have a very wide range of applications, and it's cool to measure just by adding a magnet!

    A company that has made a very high accuracy motor driver for us told me that they're primarily using IC's from IC-Haus: http://www.ichaus.de/keyword/Magnetic%20Encoder%20iCs.

    This company is also interesting: http://www.rls.si/en/am512b-9-bit-rotary-magnetic-sensor-chip--15882#ElementMediaList40407