Sensors
  • Technologies
  • More
Sensors
Sensor Forum Driving the ultrasonic transducer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 350 subscribers
  • Views 822 views
  • Users 0 members are here
Related

Driving the ultrasonic transducer

e14 Contributor
e14 Contributor over 12 years ago

I am building an ultrasonic transmitter using prowave 400fs080 .It offers 360 degree beam directivity . I have got the datasheet(  http://www.datasheetlib.com/datasheet/1154043/400fs080_pro-wave-electronics.html ) of the transducer and it says that the maximum drive voltage is 150 vp-p for burst and the resonant frequency is 40khz. To produce such a signal ,I thought of using an opamp(741) multivibrator to produce the 40 khz square wave(Vpp - 24v) and connecting  it to a primary of step up transformer(24v -120v).Will this work and what would be the current needed to drive the transducer.I cannot find the minimum  or maximum current rating in the datasheet .How will the drive voltage and current  affect the transmission ?

  • Sign in to reply
  • Cancel
Parents
  • imahusin
    imahusin over 9 years ago

    Hello MR Sambandam, I'm also having the same problem with you.

    1 How to determine the voltage and current required to drive the ultrasonic transducer I'm using  MCUSR18A40B12RSMCUSR18A40B12RS The data sheet just tell about the Allowable Input voltage

    2. The datasheet stated that the detectable range is 0.1 to 3.0m. If I want to measure less that the range, can the transducer working?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • imahusin
    imahusin over 9 years ago

    Hello MR Sambandam, I'm also having the same problem with you.

    1 How to determine the voltage and current required to drive the ultrasonic transducer I'm using  MCUSR18A40B12RSMCUSR18A40B12RS The data sheet just tell about the Allowable Input voltage

    2. The datasheet stated that the detectable range is 0.1 to 3.0m. If I want to measure less that the range, can the transducer working?