Sensors
  • Technologies
  • More
Sensors
Sensor Forum Powering analog sensors with digital output pins
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 350 subscribers
  • Views 577 views
  • Users 0 members are here
Related

Powering analog sensors with digital output pins

e14 Contributor
e14 Contributor over 11 years ago

I have an application where I need to hookup 10-12 hall effect sensors to an Arduino mega - each sensor consumes ~7mA.  I would like to power the unit from a large-ish LiPo battery and am curious as to the pros/cons of powering the sensors from the +5V pin or from digital pins set as outputs?  It seems like using digital pins would allow me to control when I actually power the sensors and provide greater flexibility in terms of maximizing runtime.  Are there any drawbacks to this approach - I am assuming that the pins provide a reliable 5V source when set as an output?  Any insight would be appreciated!

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 11 years ago

    I've done this (or similar things) often. You have to be careful that the digital output pins can cope with the current and, in addition, that the voltage drop at the current in question is OK. Digital output pins are often a little noisier than the supply and the voltage drop is often modulated a little by operation of other circuits on the chip .

    Despite all this it can often be  a very cost effective method of controlling power.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago

    I've done this (or similar things) often. You have to be careful that the digital output pins can cope with the current and, in addition, that the voltage drop at the current in question is OK. Digital output pins are often a little noisier than the supply and the voltage drop is often modulated a little by operation of other circuits on the chip .

    Despite all this it can often be  a very cost effective method of controlling power.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    Thanks Michael!  That's what I needed to know.  Much appreciated.