Sensors
  • Technologies
  • More
Sensors
Sensor Forum Rough environment rotation speed sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 354 subscribers
  • Views 1744 views
  • Users 0 members are here
Related

Rough environment rotation speed sensor

e14 Contributor
e14 Contributor over 11 years ago

Hello altogether,

 

I want to measure the rotation speed of a auxiliary fan which is enclosed in a duct pipe system.

There will be humidity and steam from boiling water (can compare to cooking on a gas hob in the kitchen)

 

The fan blades are made of plastic.

 

I was recommended to use an optical sensor, but I am worried that the steam will interfere.

 

Has anybody experience with something like this and can recommend a certain type of sensor or maybe even a special product?

 

Thanks guys!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom +2
    I am worried that the steam will interfere If the pipe is that full of steam, I think the plastic blades will be the biggest issue. Many of the sensors use IR and work at very close distances. You might…
  • tekmeister
    tekmeister over 11 years ago +1
    Optical might work, but I'd be looking at using a laser. Any chance you can swap the fan motor out to one that provides feedback via a 3rd wire?
  • tekmeister
    tekmeister over 11 years ago in reply to gadget.iom +1
    I was going to mention hall effect sensors. The reason I went with reed switches was because they operate over a wider temperature range, but I suppose for steam (~100 degrees C) hall effect will be fine…
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    If you do choose to go down the Magnetic route, you might want to look at Hall Effect magnetic sensors over reed switches. The solid state nature of a Hall effect device will typically outlive the mechanical operation of a reed switch, Especially with the number of operations you are expecting.

     

    A reed switch may have issues keeping up with the high speed switching if operating three times per revolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 11 years ago

    If you do choose to go down the Magnetic route, you might want to look at Hall Effect magnetic sensors over reed switches. The solid state nature of a Hall effect device will typically outlive the mechanical operation of a reed switch, Especially with the number of operations you are expecting.

     

    A reed switch may have issues keeping up with the high speed switching if operating three times per revolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom

    I am worried that the steam will interfere

    If the pipe is that full of steam, I think the plastic blades will be the biggest issue.

     

    Many of the sensors use IR and work at very close distances.

    You might need to provide an IR reflective surface on the blades, which will ensure the contrast to the background is increased.

     

    I'm sure that a sender on one side, and receiver on the other side of the blade will be more than suitable to overcome any steam..

     

     

    As this is a fan to be run at a determined airflow

    Out of interest why are you worried about the speed ... surely measuring the flow is more important.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • tekmeister
    tekmeister over 11 years ago in reply to gadget.iom

    I was going to mention hall effect sensors. The reason I went with reed switches was because they operate over a wider temperature range, but I suppose for steam (~100 degrees C) hall effect will be fine.

     

    A previous project I was involved in needed to measure rotational speeds in environments of 300+ degrees C. We used multiple reed switches for redundancy/reliability.