Sensors
  • Technologies
  • More
Sensors
Sensor Forum Help with 5883L crazyness.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 350 subscribers
  • Views 5292 views
  • Users 0 members are here
  • 5883l
Related

Help with 5883L crazyness.

screamingtiger
screamingtiger over 11 years ago

shabaz

jw0752

 

I have collected data and cannot get it to point to the correct heading.  Its off quite a bit and I cannot adjust as the amount it is off is non-linear.  For example, at 0 degrees it shows 100 degrees.  But at 45 degrees it shows 170 degrees.  Z axis is level and remain constant for the most part.

 


Here is the data I collected, does it makes sense?  I used a compass on my phone and compared to the readings I am getting.

 

 

 

0 degrees North
X 0
Y 155
Z -530

 

Calculated heading: 100

 

 

90 degrees east

 

X -165
Y 100 (shouldn't this read 0 since it is pointing in same direction X was just at?)
Z -530
Calculated Heading: 224

 


180 degress South
X: 0
Y: -290
Z: -540

 

Calculating Heading: 286

 

 

 

270 degrees West

 

X: 250
Y: -100
Z: -550
Calculated Heading: 252

 


One thing I am thinking is odd, if at 0 degrees north X axis reads 0, if I rotate 90 degrees to right, would Y axis now read 0?

 

I am not sure what the axis is measuring, I thought it was force and it I point x axis in one direction, then Y axis in same direction, they would show the same reading...

 

X and Y are 90 degrees in parallel plane.
I ordered another magnometer hoping a different brand will help.  Its still 5883L but different maker of breakout.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to screamingtiger +2
    Hi Joey, I took your code and added ALG_TEST stuff to it and modifying the declinationAngle variable: //#include "heading.h" #include <stdio.h> #include <iostream> //#include <wiringPi.h> //#include…
  • jw0752
    jw0752 over 11 years ago +1
    Hi Joey, This may be off base but if I treat your X and Y data as vectors and calculate Result = Sqrt( X^2 + Y^2) I get a Result that is at least in the ball park for the headings that you listed. Like…
  • jw0752
    jw0752 over 11 years ago +1
    Ok now you can see I really don't grasp it quickly as that is exactly what you were doing. No wonder my calculations matched yours. I will put my thinking cap back on and let you know if something better…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    I am tempted to erase my first two replies but I have learned from past experience that even bad advice can sometimes trigger an insight. If I take the dot product of the values of your test I get the following numbers:

    North:   552.20

    East      564.02

    South   612.94

    West    612.37

    If the magnetometer is measuring the strength of the field it is expected that we would have the same number with the dot product of the vectors regardless of the orientation of the magnetometer.  These numbers are close particularly the South and West. I assumed that your angles were precisely 90 degrees as the numbers were crunched using the easy Pythagorean Equation. This would seem to indicate that the magnetometer is working correctly and it is a mathematical translation problem. I am guessing that the N and E were not precisely at right angles and so my calculations would have been off for them.

    Sorry for the inundation of ideas but I use this as a problem solving method.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    I am tempted to erase my first two replies but I have learned from past experience that even bad advice can sometimes trigger an insight. If I take the dot product of the values of your test I get the following numbers:

    North:   552.20

    East      564.02

    South   612.94

    West    612.37

    If the magnetometer is measuring the strength of the field it is expected that we would have the same number with the dot product of the vectors regardless of the orientation of the magnetometer.  These numbers are close particularly the South and West. I assumed that your angles were precisely 90 degrees as the numbers were crunched using the easy Pythagorean Equation. This would seem to indicate that the magnetometer is working correctly and it is a mathematical translation problem. I am guessing that the N and E were not precisely at right angles and so my calculations would have been off for them.

    Sorry for the inundation of ideas but I use this as a problem solving method.

    John