Sensors
  • Technologies
  • More
Sensors
Sensor Forum Bottle counter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 352 subscribers
  • Views 3132 views
  • Users 0 members are here
Related

Bottle counter

e14 Contributor
e14 Contributor over 10 years ago

Hi, Im trying to find a suitable sensor to count bottles as they pass on a conveyor.  I want to connect it to an RPi, with PiFace.  Any help would be appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • kas.lewis
    kas.lewis over 10 years ago in reply to e14 Contributor +1
    Personally I have never used a RPi as I feel for almost anything i do it's over kill. If it is a simple project why not use Arduino (not that I have used that much either). Other options are TI Launchpads…
  • gadget.iom
    gadget.iom over 10 years ago in reply to e14 Contributor +1 suggested
    To be honest, for a task this simple I would use a basic microcontroller. it can be done on an Arduino much easier and with fewer external components. Take a look at the following article. It pretty much…
Parents
  • kas.lewis
    0 kas.lewis over 10 years ago

    ST recently came out with their flight sence sensor that measures distance (to 50 cm) pretty accurately and they are decently priced as well. That would be an easy way to use a beam breaker but with only needing to position one sensor, it uses I2C.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 10 years ago

    ST recently came out with their flight sence sensor that measures distance (to 50 cm) pretty accurately and they are decently priced as well. That would be an easy way to use a beam breaker but with only needing to position one sensor, it uses I2C.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to kas.lewis

    Thanks Paul & Kas, that's given me something to work with.  Do either of you know of any good resources in terms of software to use them with?  I'm pretty new to using an RPi for this kind of application, so it's quite a steep learning curve for me.

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 10 years ago in reply to e14 Contributor

    Personally I have never used a RPi as I feel for almost anything i do it's over kill. If it is a simple project why not use Arduino (not that I have used that much either). Other options are TI Launchpads, Freescale Frdm Boards or even ST Nucleo Boards that comes with a free Keil License for the ARM M0. The ST option would allow you to get the X-NUCLEO-6180XA1 that had the flightsense on the board already. I belive the later two boards can be programed in mbed and the first board can be done in Energia, which is like arduino but for TI boards, all teh boards can be programed in C. I hope that helps a bit.

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to kas.lewis

    Thanks for the info Kas. The main reason I'm trying this with an RPi is purely because I have one laying around and I'm reasonably familiar with it. I knew there were other options out there but I know pretty much zero about them lol