Sensors
  • Technologies
  • More
Sensors
Sensor Forum Using Hall Effect Sensors Paired With SMD Inductors For Data Transmission...Feasible?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 351 subscribers
  • Views 2643 views
  • Users 0 members are here
  • data_transmission
  • hall_effect_sensors
  • short_range_wireless
  • magneticsensor
  • magnetism
Related

Using Hall Effect Sensors Paired With SMD Inductors For Data Transmission...Feasible?

andysrobotics
andysrobotics over 10 years ago

Hi All,

 

I have an application where I need very short range data transmission (up to 2cm).

Any higher and this adds too much complexity and cost to the project due to many identical objects in very close vicinity of each other.

 

Originally this was going to be designed using IR for a two way link but the project must be waterproof.

 

I was thinking of both the master device and slave devices having a electromagnet for the transmitter and a hall effect sensor for the receiver.

The RX and TX are far enough apart (10cm) to not interfere with each other.

 

Each side will have a pair of transmitters and receivers - this is to allow for multiple orientation - using neodymium magnets to help with alignment.

having a pair of channels also allows for a unconventional SPI comms.

Master TX1 -> Slave RX1 = Master controlled CS (Master will have multiple slaves)

Master TX2 -> Slave RX2 = MOSI data

Master RX1 <- Slave TX1 = Slave Generated Data Clock (unconventional but allows for multiple orientation)

Master RX2 <- Slave TX2 = MISO data

 

The data rate can be low - as low as 1200bps (or less) as there will only be about 30 bytes per transmission and only 1 transmission per second.

 

My questions are...will this work?

What range does a hall effect sensor have?

Are small SMD inductors capable of producing enough magnetism for the sensors to pick up - through waterproof material?

Will an inductor hold magnetic charge and prevent data style pulses from being read?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +2 suggested
    Yes what you want to do is feasible. Several inductive wireless charging systems (like Qi, PMA and A4WP) already embed data transfer in the power signal. PMA in particular seems to to be opening up communications…
  • dougw
    dougw over 10 years ago in reply to andysrobotics +1
    Here is a project by David McIntosh using MSP430: https://sites.google.com/site/ddmcintosh2projects/inductive-charger
Parents
  • dougw
    0 dougw over 10 years ago

    Yes what you want to do is feasible.

    Several inductive wireless charging systems (like Qi, PMA and A4WP) already embed data transfer in the power signal. PMA in particular seems to to be opening up communications. They don't need Hall sensors since the power scavenging circuit (coil) is enough to transfer/capture everything.

    NFC/RFID can also be used for both power and data transfer, and it isn't too hard to rig up your own scheme.

    TransferJet plans to merge NFC, higher speed communications and wireless charging - Sony is already making TransferJet chips.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 10 years ago in reply to dougw

    Isn't that the definition of radio?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to D_Hersey

    I guess it could be called radio, but the power transfer is mostly done with magnetic fields, like through a transformer, and the data is often transferred by modulating the magnetic field. Essentially an air core transformer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 10 years ago in reply to D_Hersey

    As Doug says, most of these systems use mutual inductance between coils. If you want to think about it in radio terms, that's the near field (storage field) that exists close to the antenna. The coils are small (in wavelength terms) and don't radiate much.

     

    Signalling in the forward direction is by modulating the field. In the back direction it's by loading the field; the receiver will short or partially short its coil momentarily and the supply current to the oscillator that's driving the transmit coil will increase and can be sensed (you can't do that with a propagating wave where the transmitter has no idea at all whether the energy has been absorbed somewhere, in some far off place, or not).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 10 years ago in reply to D_Hersey

    As Doug says, most of these systems use mutual inductance between coils. If you want to think about it in radio terms, that's the near field (storage field) that exists close to the antenna. The coils are small (in wavelength terms) and don't radiate much.

     

    Signalling in the forward direction is by modulating the field. In the back direction it's by loading the field; the receiver will short or partially short its coil momentarily and the supply current to the oscillator that's driving the transmit coil will increase and can be sensed (you can't do that with a propagating wave where the transmitter has no idea at all whether the energy has been absorbed somewhere, in some far off place, or not).