Sensors
  • Technologies
  • More
Sensors
Sensor Forum When you need many sensors at once...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 4 answers
  • Subscribers 355 subscribers
  • Views 5424 views
  • Users 0 members are here
Related

When you need many sensors at once...

screamingtiger
screamingtiger over 10 years ago

I have a project where I may need 25+ accelerometers and magnetometers.

 

I see three options for sensors:

-Direct wire, which could be possible with shift registers

-I2c, however many sensors of the same brand only ship with 1 or 2 address options and I dont want to have dozens of different brands with with different protocols

-SPI, same problem as I2c.

 

I found the I2C sensors to be cheap, is there a way to use numerous sensors with the same address within one bus?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +4 verified
    Linear Technology makes chips to handle this situation - up to 127 devices with the same address can be handled on one bus, but you may need one of these chips at each sensor. They cost about $2 each.…
  • shabaz
    shabaz over 10 years ago in reply to gdstew +2 suggested
    yet here you are again pushing the easily dis-proven idea that I2C is only good for short distances between boards Where did I state with the explicitness that you suggest, that it is only good for short…
  • michaelkellett
    michaelkellett over 10 years ago in reply to screamingtiger +2
    Another method you might consider (it's cheaper for the parts but has other issues) would be to use a single micro with plenty of pins (50 spare IOs needed) and bit bang as many IC2 buses as you need.…
Parents
  • kulky64
    0 kulky64 over 10 years ago

    I would put all sensors on the same I2C bus and make some address decoder to make only one device active at a time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to kulky64

    Do you have a  decoder example, kulky64?

    I'd be interested in a usable example too (not looking for 25+ sensors, but would be helped if you know one for using two fixed-address ICs).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kulky64
    0 kulky64 over 10 years ago in reply to Jan Cumps

    If you have device with only one fixed address, then this is not usable. But if device has at least one hardware pin to set I2C address, then it should be possible to dynamically change logic level on that pin(s) using some spare GPIOs or logic decoder to make only one responding to MCU. This may not be usable to all I2C devices. For example if device scans logic level on its address pin only during power-up or reset and then assumes that address until next power-up/reset.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kulky64
    0 kulky64 over 10 years ago in reply to Jan Cumps

    If you have device with only one fixed address, then this is not usable. But if device has at least one hardware pin to set I2C address, then it should be possible to dynamically change logic level on that pin(s) using some spare GPIOs or logic decoder to make only one responding to MCU. This may not be usable to all I2C devices. For example if device scans logic level on its address pin only during power-up or reset and then assumes that address until next power-up/reset.