Sensors
  • Technologies
  • More
Sensors
Sensor Forum When you need many sensors at once...
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 4 answers
  • Subscribers 355 subscribers
  • Views 5402 views
  • Users 0 members are here
Related

When you need many sensors at once...

screamingtiger
screamingtiger over 10 years ago

I have a project where I may need 25+ accelerometers and magnetometers.

 

I see three options for sensors:

-Direct wire, which could be possible with shift registers

-I2c, however many sensors of the same brand only ship with 1 or 2 address options and I dont want to have dozens of different brands with with different protocols

-SPI, same problem as I2c.

 

I found the I2C sensors to be cheap, is there a way to use numerous sensors with the same address within one bus?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +4 verified
    Linear Technology makes chips to handle this situation - up to 127 devices with the same address can be handled on one bus, but you may need one of these chips at each sensor. They cost about $2 each.…
  • shabaz
    shabaz over 10 years ago in reply to gdstew +2 suggested
    yet here you are again pushing the easily dis-proven idea that I2C is only good for short distances between boards Where did I state with the explicitness that you suggest, that it is only good for short…
  • michaelkellett
    michaelkellett over 10 years ago in reply to screamingtiger +2
    Another method you might consider (it's cheaper for the parts but has other issues) would be to use a single micro with plenty of pins (50 spare IOs needed) and bit bang as many IC2 buses as you need.…
Parents
  • screamingtiger
    0 screamingtiger over 10 years ago

    I need to take multiple G readings across a device that is a cube about 1-2 feet.

     

    I do know that I2C has its limitations, but in practice it works well for a protocol for external sensors.

     

    I could attach an Arduino or some MCU to each sensor and then use serial across the MCUs but that is a waste just to "follow the rules"  image

     

    I'm going to look into the multiplexor!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to screamingtiger

    Going beyond i2c's limits - particularly at lower speeds - is possible, screamingtiger. But I concur with shabaz that this is a stretch: can be done, but at a cost/risk.

    I think that using a protocol outside its original habitat is an advanced topic.

    I always respect people that get more out of something than the original designers intended.

    But also feel that it shouldn't be the first design option when engineering something.

    Stretching protocols for your need would almost be a last resort....

     

    Keep us posted on the multiplexer, please.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to screamingtiger

    Going beyond i2c's limits - particularly at lower speeds - is possible, screamingtiger. But I concur with shabaz that this is a stretch: can be done, but at a cost/risk.

    I think that using a protocol outside its original habitat is an advanced topic.

    I always respect people that get more out of something than the original designers intended.

    But also feel that it shouldn't be the first design option when engineering something.

    Stretching protocols for your need would almost be a last resort....

     

    Keep us posted on the multiplexer, please.