Sensors
  • Technologies
  • More
Sensors
Sensor Forum Omron 2SMPP-02 Pressure Sensor - reading goes down over time
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 349 subscribers
  • Views 2380 views
  • Users 0 members are here
Related

Omron 2SMPP-02 Pressure Sensor - reading goes down over time

johnsandhu@comcast.net
johnsandhu@comcast.net over 9 years ago

We've been noticing that when an Omron  2SMPP-022SMPP-02 sensor is put under even a very small pressure the reading goes down over time We've checked for leaks in the system and ruled those out We know the reading is very stable at zero pressure Our application is a water level sensor The tube is 10 feet long 1/4 inch diameter so the exposure of the air in the tube to water is fairly low although even at room temp you would expect some water vapor pressure to be present The question we have is whether the reduction in pressure reading from the MEMs sensor is due to the water vapor building up or is it due to something else we are not considering We do have a temperature sensor and are ruling out all temperature related effects The pressures we operate under are only about 2 to 10 kPA The sensor is rated at 37 kPA Data on sensors is not clear on affects of small amounts of water vapor

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +1 suggested
    Hi John, Before you do too much guessing it would be a good idea to determine whether the change is in the pressure itself, the sensor, or the electronics associated with the sensor. You can monitor low…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi John,

     

    Before you do too much guessing it would be a good idea to determine whether the change is in the pressure itself, the sensor, or the electronics associated with the sensor. You can monitor low pressures like this with a manometer:

     

    image

     

    I would recommend putting a manometer on the system and mark the level indicated and note the pressure indicated by the sensor. Return later and check the two again. The manometer will only be as inaccurate as you are able to read it. In my experience water that is left to sit will increase its specific gravity slightly as it looses gas content. For the same level of water this would translate to a slight increase in pressure. If it is a closed system your vapor pressure may also make a contribution to raising the  pressure. Both of these things are counter to your experience of a lowering pressure indication. Make sure your electronics are warmed up to operating temperature before you do your calibrations. Make sure your voltage reference for the sensor is stable. I will add more if I can think of more.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi John,

     

    Before you do too much guessing it would be a good idea to determine whether the change is in the pressure itself, the sensor, or the electronics associated with the sensor. You can monitor low pressures like this with a manometer:

     

    image

     

    I would recommend putting a manometer on the system and mark the level indicated and note the pressure indicated by the sensor. Return later and check the two again. The manometer will only be as inaccurate as you are able to read it. In my experience water that is left to sit will increase its specific gravity slightly as it looses gas content. For the same level of water this would translate to a slight increase in pressure. If it is a closed system your vapor pressure may also make a contribution to raising the  pressure. Both of these things are counter to your experience of a lowering pressure indication. Make sure your electronics are warmed up to operating temperature before you do your calibrations. Make sure your voltage reference for the sensor is stable. I will add more if I can think of more.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer