Sensors
  • Technologies
  • More
Sensors
Sensor Forum Struggling to get a digital sensor to see my indoor ambient light
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 350 subscribers
  • Views 2078 views
  • Users 0 members are here
  • light sensor
  • photodiode
  • ambient light sensor
  • photoresistor
Related

Struggling to get a digital sensor to see my indoor ambient light

suitcase
suitcase over 6 years ago

I wanted to use a Raspberry Pi to check whether my room's ceiling light was on. I’m an electronics amateur and do not want to solder anything, so I am using a Pi Zero W with presoldered pins, and using female-to-female Dupont cables I bought to connect the GPIO pins to the sensor board.

 

I bought this cheap little photoresistor board: https://www.aliexpress.com/item/32806322505.html

 

I set it up successfully (using the digital out, since a regular Pi can't see analog signals). I can easily set it up so that flashing my phone flashlight at it will make it return something different over the digital out.

 

But with all the adjusting I'm doing of the potentiometer, I just can't get it to reliably trigger when the ambient room light changes. If I am REALLY careful with it, tweaking the potentiometer to the point the “DO-LED” starts flickering on and off, barely turning on, I can get it to work for a few minutes to return 1 or 0 over the digital output based on the room’s light, but it’s very flaky. Right now I just thought I got it right, but after five minutes, find it’s flickering between 0 and 1 again.

 

What would be a better, more reliable room sensor I could purchase? I bought a similar board that used a photodiode instead, and it's just as bad. Maybe worse, because photodiodes are more directional, I guess. It just seems like these little potentiometer-adjustable sensors have a microscopic “sweet spot” for detecting ambient room light, which doesn’t make sense to me.

 

One critical thing is that I don’t want to solder anything, or use a breadboard, or anything that seems complicated. I really liked my little setup with the dupont cables and this board, and I’d like something that is just as doable with my hands alone. What should I get?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +7 suggested
    Hi, You might want to check to see if you can find a module that has a hysteresis adjustment as well as a sensitivity control. The hysteresis will allow you to adjust the turn on and turn off points to…
  • dougw
    dougw over 6 years ago +6 suggested
    You could try putting a little cup reflector around the sensor to collect more light onto the sensor surface. something like aluminum foil should work, but be careful not to short out the sensor leads…
  • fmilburn
    fmilburn over 6 years ago +5 suggested
    There are more precise sensors like the one by Rohm that is included in the RoadTest here . Adafruit also sells one that I have used. They should be relatively easy to set up over I2C on the Pi although…
Parents
  • dougw
    0 dougw over 6 years ago

    You could try putting a little cup reflector around the sensor to collect more light onto the sensor surface. something like aluminum foil should work, but be careful not to short out the sensor leads with the foil. A little hot glue or silicone glue would insulate the leads. An alternative is simply a white paper reflector.

    You can carefully bend the sensor leads so the sensor faces up if that helps.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 6 years ago

    You could try putting a little cup reflector around the sensor to collect more light onto the sensor surface. something like aluminum foil should work, but be careful not to short out the sensor leads with the foil. A little hot glue or silicone glue would insulate the leads. An alternative is simply a white paper reflector.

    You can carefully bend the sensor leads so the sensor faces up if that helps.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • suitcase
    0 suitcase over 6 years ago in reply to dougw

    Ah, I appreciate it! Honestly, I’m a bit cold on the idea of adding something like a cone to it because I wanted it to be less fussy than my old setup, which was with this thing in a shoebox with a cheap fresnel lens carefully aimed at the ceiling light. But it’s an ingenious idea, the kind I am certainly looking for image