Sensors
  • Technologies
  • More
Sensors
Sensor Forum Looking for novel ways to create an air flow for dust or air quality sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 14 answers
  • Subscribers 349 subscribers
  • Views 5091 views
  • Users 0 members are here
  • air quality sensor
  • dust sensor
  • air particulates
Related

Looking for novel ways to create an air flow for dust or air quality sensor

BigG
BigG over 6 years ago

I'm looking at various dust sensors for a home monitoring application - one location would be a bedroom.

 

I noticed that some of these sensors, such as Omron's B5W-LD0101 sensor, for example, include a resistor inside the sensor which acts as a heater to generate an air flow or air drift past the optical sensor which then measures the particulate density.

 

Some others, such as Sharp's GP2Y10## do not include heaters.

 

The Sharp sensor is attractive because of low cost.

 

I now want to explore novel ways to generate air flow to improve measurement quality with a Sharp Air Quality sensor.

 

One idea I had, but have not sure if it would work, was to use an ultrasonic sensor, such as the cheap HC-SR04 to gently agitate a surface to "move" air flow through the inlet. I know you get ultrasonic cleaners but I thought that if the ultrasonic pulse is low power it certainly won't clean but maybe it would at least agitate air / dust particulates a little etc. I also liked this idea as the ultrasonic sensor could maybe be placed a couple of centimetres away. With resistors generating heat, I would assume the resistor has to be placed right at the inlet which is not always possible.

 

I know another obvious option is a small fan run off a dc motor but that would be noisy and not suitable at night, especially in a bed room.

 

Any other ideas or thoughts on this topic.

 

I look forward to feedback.

 

Thanks

 

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +7 suggested
    You could check out piezo fans - they are small, low power and quiet.
  • shabaz
    shabaz over 6 years ago +6 suggested
    Hi Colin, I think Murata have a micro blower, which possibly uses piezo tech (not sure). I've not used it, so I don't know if it is almost silent or not, or how well it would work with the dust sensors…
  • genebren
    genebren over 6 years ago +5 suggested
    The Murata Microblowers might work, but they are neither cheap or trivial to drive. I used the MZB1001T02 parts on a project for a client, which ended up using full H-bridges to provide the 10 to 20 Vpkpk…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    Farnell have a range of tiny fans, 11 of them <= 17mm square.

     

    2856028 is 16mm square and 4mm thick, noise 3dBA, £5.95, looks like a good choice.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 6 years ago in reply to michaelkellett

    Thanks MK. I had a quick look on Farnell. It's a nice compact size and the right operating voltage. I see it's quite a "whizzy" little fan with rpm at 6500 rpm, generating a flow rate of 0.012m³/min, which may mean it needs to be quite close to the dust sensor inlet or put inside a funnel. I'm still a little reluctant to use a fan because if my computer fan is anything to go by, it eventually accumulates dust on the blades, making it noisier. But for that price it won't do any harm trying it out.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to BigG

    I think anything you use to pump air will collect dust. The heaters may be a bit less affected (ie they'll still work when dusty) but I think the piezo ' fans ' are mechanically tuned so will work less well when dirty.

    The tiny rotary fans may well get noisy when dirty but this one is slower and quieter than many.

    You could design a heater based pump that was easily washable.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 6 years ago in reply to BigG

    I think anything you use to pump air will collect dust. The heaters may be a bit less affected (ie they'll still work when dusty) but I think the piezo ' fans ' are mechanically tuned so will work less well when dirty.

    The tiny rotary fans may well get noisy when dirty but this one is slower and quieter than many.

    You could design a heater based pump that was easily washable.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer