Sensors
  • Technologies
  • More
Sensors
Sensor Forum Looking for novel ways to create an air flow for dust or air quality sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 14 answers
  • Subscribers 349 subscribers
  • Views 5122 views
  • Users 0 members are here
  • air quality sensor
  • dust sensor
  • air particulates
Related

Looking for novel ways to create an air flow for dust or air quality sensor

BigG
BigG over 6 years ago

I'm looking at various dust sensors for a home monitoring application - one location would be a bedroom.

 

I noticed that some of these sensors, such as Omron's B5W-LD0101 sensor, for example, include a resistor inside the sensor which acts as a heater to generate an air flow or air drift past the optical sensor which then measures the particulate density.

 

Some others, such as Sharp's GP2Y10## do not include heaters.

 

The Sharp sensor is attractive because of low cost.

 

I now want to explore novel ways to generate air flow to improve measurement quality with a Sharp Air Quality sensor.

 

One idea I had, but have not sure if it would work, was to use an ultrasonic sensor, such as the cheap HC-SR04 to gently agitate a surface to "move" air flow through the inlet. I know you get ultrasonic cleaners but I thought that if the ultrasonic pulse is low power it certainly won't clean but maybe it would at least agitate air / dust particulates a little etc. I also liked this idea as the ultrasonic sensor could maybe be placed a couple of centimetres away. With resistors generating heat, I would assume the resistor has to be placed right at the inlet which is not always possible.

 

I know another obvious option is a small fan run off a dc motor but that would be noisy and not suitable at night, especially in a bed room.

 

Any other ideas or thoughts on this topic.

 

I look forward to feedback.

 

Thanks

 

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +7 suggested
    You could check out piezo fans - they are small, low power and quiet.
  • shabaz
    shabaz over 6 years ago +6 suggested
    Hi Colin, I think Murata have a micro blower, which possibly uses piezo tech (not sure). I've not used it, so I don't know if it is almost silent or not, or how well it would work with the dust sensors…
  • genebren
    genebren over 6 years ago +5 suggested
    The Murata Microblowers might work, but they are neither cheap or trivial to drive. I used the MZB1001T02 parts on a project for a client, which ended up using full H-bridges to provide the 10 to 20 Vpkpk…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    Farnell have a range of tiny fans, 11 of them <= 17mm square.

     

    2856028 is 16mm square and 4mm thick, noise 3dBA, £5.95, looks like a good choice.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to michaelkellett

    Wow. I've never seen a fan so tiny or with such a low noise rating. I'm tempted to order it too, just to see it! : )

     

    This reminds me, I opened up a network storage unit last week, and I took a photo of the fan. Reason being, I was impressed with it.. it's been running for more than 8 years, and had finally stopped spinning. I blew the dust off it using a spray can, and now it's running again. I have an alternative replacement fan, but since this one has been so reliable, I felt perhaps I shouldn't change it out yet.. (it's safe, the network storage will auto-shut-down if the fan stops spinning). The spinning disk has 8 years of uptime too! (it has nothing critical on it, so that won't get swapped out yet either).

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago in reply to michaelkellett

    Wow. I've never seen a fan so tiny or with such a low noise rating. I'm tempted to order it too, just to see it! : )

     

    This reminds me, I opened up a network storage unit last week, and I took a photo of the fan. Reason being, I was impressed with it.. it's been running for more than 8 years, and had finally stopped spinning. I blew the dust off it using a spray can, and now it's running again. I have an alternative replacement fan, but since this one has been so reliable, I felt perhaps I shouldn't change it out yet.. (it's safe, the network storage will auto-shut-down if the fan stops spinning). The spinning disk has 8 years of uptime too! (it has nothing critical on it, so that won't get swapped out yet either).

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dubbie
    0 dubbie over 6 years ago in reply to shabaz

    I don't think I have anything electronic that is 8 years old. I consider anything lasting longer than 3 years a bonus! Still, I hope my DSO (GDS-1052-U) lasts a long time as I've had it nearly three years already. Come to think of it I would like my 3D printer to last longer than 3 years as well, also currently coming up to its third birthday.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 6 years ago in reply to shabaz

    I like the "dust off it using a spray can" method. I have a Dell Vostro 400 that is now  almost 12 years old and is still being used daily. The fans got rather clogged up with dust and got very noisy. Have to clean with an old toothbrush when the dust gets caked on. They all still working though. I now pat the PC daily as sign of appreciation as its an amazing machine considering the hours its put in. Sadly, it's days are numbered as 32bit windows computing is dying off slowly.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kmikemoo
    0 kmikemoo over 6 years ago in reply to shabaz

    While I also like the dusting by spray can method, I have learned to move the item outside before pulling the trigger.  No amount of vacuuming seems to be enough to prevent the inevitable dust fog from the initial blasts

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to kmikemoo

    Hehe I was just going to mention that! Going outside is an important part of the process and very easy to miss the first time around, for trigger-happy spray-can users : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 6 years ago in reply to kmikemoo

    Aaaagh, a case of "I wouldn't have thought of that"... now I know.

     

     

    via GIPHY

    • Cancel
    • Vote Up +3 Vote Down