Sensors
  • Technologies
  • More
Sensors
Sensor Forum Looking for novel ways to create an air flow for dust or air quality sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 14 answers
  • Subscribers 349 subscribers
  • Views 5091 views
  • Users 0 members are here
  • air quality sensor
  • dust sensor
  • air particulates
Related

Looking for novel ways to create an air flow for dust or air quality sensor

BigG
BigG over 6 years ago

I'm looking at various dust sensors for a home monitoring application - one location would be a bedroom.

 

I noticed that some of these sensors, such as Omron's B5W-LD0101 sensor, for example, include a resistor inside the sensor which acts as a heater to generate an air flow or air drift past the optical sensor which then measures the particulate density.

 

Some others, such as Sharp's GP2Y10## do not include heaters.

 

The Sharp sensor is attractive because of low cost.

 

I now want to explore novel ways to generate air flow to improve measurement quality with a Sharp Air Quality sensor.

 

One idea I had, but have not sure if it would work, was to use an ultrasonic sensor, such as the cheap HC-SR04 to gently agitate a surface to "move" air flow through the inlet. I know you get ultrasonic cleaners but I thought that if the ultrasonic pulse is low power it certainly won't clean but maybe it would at least agitate air / dust particulates a little etc. I also liked this idea as the ultrasonic sensor could maybe be placed a couple of centimetres away. With resistors generating heat, I would assume the resistor has to be placed right at the inlet which is not always possible.

 

I know another obvious option is a small fan run off a dc motor but that would be noisy and not suitable at night, especially in a bed room.

 

Any other ideas or thoughts on this topic.

 

I look forward to feedback.

 

Thanks

 

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +7 suggested
    You could check out piezo fans - they are small, low power and quiet.
  • shabaz
    shabaz over 6 years ago +6 suggested
    Hi Colin, I think Murata have a micro blower, which possibly uses piezo tech (not sure). I've not used it, so I don't know if it is almost silent or not, or how well it would work with the dust sensors…
  • genebren
    genebren over 6 years ago +5 suggested
    The Murata Microblowers might work, but they are neither cheap or trivial to drive. I used the MZB1001T02 parts on a project for a client, which ended up using full H-bridges to provide the 10 to 20 Vpkpk…
Parents
  • michaelkellett
    0 michaelkellett over 6 years ago

    Farnell have a range of tiny fans, 11 of them <= 17mm square.

     

    2856028 is 16mm square and 4mm thick, noise 3dBA, £5.95, looks like a good choice.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dubbie
    0 dubbie over 6 years ago in reply to michaelkellett

    I didn't know fans this small could exist. They are amazing.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to dubbie

    I'm thinking this fan could be a problem-solver for my Pi 4's.

    I am using a case that does have vents, but not a lot of space, and no significant air is moving (and I don't want a noisy fan). Maybe this would be good enough...

    I'm thinking if one doesn't make enough of an impact, then maybe two of them, in series, running off 5V.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago in reply to dubbie

    I'm thinking this fan could be a problem-solver for my Pi 4's.

    I am using a case that does have vents, but not a lot of space, and no significant air is moving (and I don't want a noisy fan). Maybe this would be good enough...

    I'm thinking if one doesn't make enough of an impact, then maybe two of them, in series, running off 5V.

    • Cancel
    • Vote Up +3 Vote Down