Sensors
  • Technologies
  • More
Sensors
Sensor Forum Looking for novel ways to create an air flow for dust or air quality sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 14 answers
  • Subscribers 349 subscribers
  • Views 5091 views
  • Users 0 members are here
  • air quality sensor
  • dust sensor
  • air particulates
Related

Looking for novel ways to create an air flow for dust or air quality sensor

BigG
BigG over 6 years ago

I'm looking at various dust sensors for a home monitoring application - one location would be a bedroom.

 

I noticed that some of these sensors, such as Omron's B5W-LD0101 sensor, for example, include a resistor inside the sensor which acts as a heater to generate an air flow or air drift past the optical sensor which then measures the particulate density.

 

Some others, such as Sharp's GP2Y10## do not include heaters.

 

The Sharp sensor is attractive because of low cost.

 

I now want to explore novel ways to generate air flow to improve measurement quality with a Sharp Air Quality sensor.

 

One idea I had, but have not sure if it would work, was to use an ultrasonic sensor, such as the cheap HC-SR04 to gently agitate a surface to "move" air flow through the inlet. I know you get ultrasonic cleaners but I thought that if the ultrasonic pulse is low power it certainly won't clean but maybe it would at least agitate air / dust particulates a little etc. I also liked this idea as the ultrasonic sensor could maybe be placed a couple of centimetres away. With resistors generating heat, I would assume the resistor has to be placed right at the inlet which is not always possible.

 

I know another obvious option is a small fan run off a dc motor but that would be noisy and not suitable at night, especially in a bed room.

 

Any other ideas or thoughts on this topic.

 

I look forward to feedback.

 

Thanks

 

Colin

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 6 years ago +7 suggested
    You could check out piezo fans - they are small, low power and quiet.
  • shabaz
    shabaz over 6 years ago +6 suggested
    Hi Colin, I think Murata have a micro blower, which possibly uses piezo tech (not sure). I've not used it, so I don't know if it is almost silent or not, or how well it would work with the dust sensors…
  • genebren
    genebren over 6 years ago +5 suggested
    The Murata Microblowers might work, but they are neither cheap or trivial to drive. I used the MZB1001T02 parts on a project for a client, which ended up using full H-bridges to provide the 10 to 20 Vpkpk…
Parents
  • dubbie
    0 dubbie over 6 years ago

    You could just try to use the natural air flow within a room. The air is never really still within any room unless it is completely closed with no temperature differentials - not realistic. If there is any heating (or cooling) in a room then there will be air flow so you could try a location above (or below - floor level?)  a window, or a radiator, near an air conditioning duct or even just the door way to the room, possibly even a light bulb (LED ones still generate some heat). I have even seen the effect of air flow caused by a human body  - this was in an art exhibition where there was a large presumably very light weight balloon moving about in the room due only to the presence of people.  It was a big room too. So you could look for areas within a room which has consistent temperature differentials and then you will get an air flow. It would need very accurate temperature measurements in order to be able to do this.

     

    Dubbie

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • BigG
    0 BigG over 6 years ago in reply to dubbie

    Thanks for your suggestion.

     

    Yes, I'm not sure using natural air flow would work in all cases.

     

    My view is that dust within a room is not uniform and based on observation tends to collect in areas where there is no natural airflow to prevent settlement or air particulate concentrations. So, my thought is that if you want to develop a trigger/alert scenario you need to place a sensor in or near these locations.

     

    Nevertheless you have highlighted some great placement positions for a sensor using heat differentials within a room. I really like your observation that heat from human body and of course movement can also be used. This would make sense for placing a dust sensor below a bed, for example. Now, I wondering if it would work with a young child.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • BigG
    0 BigG over 6 years ago in reply to dubbie

    Thanks for your suggestion.

     

    Yes, I'm not sure using natural air flow would work in all cases.

     

    My view is that dust within a room is not uniform and based on observation tends to collect in areas where there is no natural airflow to prevent settlement or air particulate concentrations. So, my thought is that if you want to develop a trigger/alert scenario you need to place a sensor in or near these locations.

     

    Nevertheless you have highlighted some great placement positions for a sensor using heat differentials within a room. I really like your observation that heat from human body and of course movement can also be used. This would make sense for placing a dust sensor below a bed, for example. Now, I wondering if it would work with a young child.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dubbie
    0 dubbie over 6 years ago in reply to BigG

    I hadn't really thought where the dust particles might actually be within the room and I'm not sure how you might find this out. You would probably need some sort of 3D grid of dust sensors within a room but then they would interfere with the air flow/dust flow. It might be possible to create some sort of simulation of a room using suitable software (I have no idea how that would be done) but then every time something was moved or somebody entered the room it would all be disturbed. It is an interesting problem.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down