Sensors
  • Technologies
  • More
Sensors
Sensor Forum Another acoustics question - what will it take to develop a cough and breathing analyser
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 351 subscribers
  • Views 1866 views
  • Users 0 members are here
  • acoustic engineering
  • breathing
  • breath_monitor
  • cough analysis
Related

Another acoustics question - what will it take to develop a cough and breathing analyser

BigG
BigG over 6 years ago

Hi all

 

Following on from the valuable feedback I received from my last acoustics related question on developing a high pass filter, I wanted to open up this highly topical acoustics related question.

 

As we probably all know by now, the covid-19 coronovirus has some fairly specific symptoms, one of which is a dry cough and/or breathing difficulties.

 

As I had acoustics projects on my brain, I wondered what techniques and sensors could be used to detect a cough and with the use of machine learning and/or AI is there a means of differentiating different coughs (as well as breathing patterns). Maybe this could then eventually form some type of data set for automated monitoring.

 

I did a quick online search and this academic paper (published 2018) popped up on my search list, which is a rather useful reference: https://www.hindawi.com/journals/js/2018/9845321/

 

So, I thought this could make for an interesting community related project and hence I'm putting it out there.

 

Where does one start, for example? Does this require a low pass filter or a pass band filter? What other acoustic techniques could be used etc.

 

Similarly with breathing - what techniques and sensors would be best suited to monitor the speed and depth of breathing.

 

Any thoughts and suggestions, will be welcomed.

 

Thanks

 

Colin (BigG)

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 6 years ago +1 suggested
    Hi BigG A great discussion. I wonder if Alexa, Google and Siri could be brought in to do this? After some changes and re-training perhaps they could listen out for coughs, analyse them and make suggestions…
  • BigG
    BigG over 6 years ago in reply to 14rhb +1
    Yes indeed. That was one ideas. I certainly felt that one would at least need to start by capturing data and in order to do so you would need something that is reliable and cannot be influenced by noise…
Parents
  • BigG
    0 BigG over 6 years ago

    Thanks for all the very helpful replies.

     

    When starting off, I like to aim at developing a low cost product/system that just works.

     

    In this case I think it is a not that straight forward as a mobile phone or tablet could be readily used as a substitute to achieve the same goal, assuming the software can be developed. In my view, phones/tablets are probably the more useful for cough analysis as it can take a once off sample of a cough, while for breathing assessment a phone/tablet might not be that practicable when someone is sleeping, for example, as this requires more continuous monitoring (although if a person is sitting up it would probably work).

     

    If it is going to be a new bit of kit, which I quite like, then what components could be added (besides mic and amplifier) to our new sensor breakout board that would deliver enhancements to make it easier and more reliable for the software to come up with the correct answers.

     

    It is the hardware side that I always struggle with. So, could a decent circuit design, specific for this application, make life easier. What components could be added etc. This is the first question to look at, in my opinion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • BigG
    0 BigG over 6 years ago

    Thanks for all the very helpful replies.

     

    When starting off, I like to aim at developing a low cost product/system that just works.

     

    In this case I think it is a not that straight forward as a mobile phone or tablet could be readily used as a substitute to achieve the same goal, assuming the software can be developed. In my view, phones/tablets are probably the more useful for cough analysis as it can take a once off sample of a cough, while for breathing assessment a phone/tablet might not be that practicable when someone is sleeping, for example, as this requires more continuous monitoring (although if a person is sitting up it would probably work).

     

    If it is going to be a new bit of kit, which I quite like, then what components could be added (besides mic and amplifier) to our new sensor breakout board that would deliver enhancements to make it easier and more reliable for the software to come up with the correct answers.

     

    It is the hardware side that I always struggle with. So, could a decent circuit design, specific for this application, make life easier. What components could be added etc. This is the first question to look at, in my opinion.