Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensor for measuring Spin Rate/Angle & Velocity/Angle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 350 subscribers
  • Views 3866 views
  • Users 0 members are here
Related

Sensor for measuring Spin Rate/Angle & Velocity/Angle

e14 Contributor
e14 Contributor over 15 years ago

Hello All,

 

I have an application which requires a sensor to measure spin rate/angle and velocity/angle.  The spin rate can be anything from -6000 to 90000°/s  and the velocity anything up to 200mph.  I do not need to measure this over a period of time, just an instantaneous reading at a point in time.  The sensor would also need to measure the spin axis as well as the velocity in the X, Y & Z axes (or just the velocity and some way of determining the angular direction).  I have looked at MEMS Gyroscopes/Accelerometers but there does not seem to be anything out there that measures high enough values.  I have been advised that a "resolver to digital device" may work but am not entirely sure what these measure.  Can anyone please offer any assistance as to what may be a suitable product?

 

Many Thanks

 

Andy.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi DAB and Michael,

     

    Many Thanks for both of your replies.  Some more information regarding the specifications:

     

    -Device will need to be free with output via wireless transmission. (RF Transmitter?).

     

    -Everything (Sensor,Power Source, Wireless Transmitter will need to fit inside a space of no more than 40mm diameter).

     

    -Power, due to space constraint I envisiaged be supplied by some sort of button cell battery (1.5-3V?).

     

    -No cost constraints. (Yet!!)

     

    -Measurement will need to be made within approx. 0.03s of initial movement.


    -Max. Linear Acceleration - 134112m/s/s (67.1m/s in 0.0005s).

     

    -Max. Angular Acceleration - 3140000 rad/s/s (Not sure if this calculation is correct. I have assumed max. angular rate of 1570 rad/second is reached at the same time as max. linear speed)

     

    -I'm not yet sure about accuracy requirementsbut for now work on +/- 2% on all measurements.

     

    The values above are maximums and maximun linear/angular speeds will not occur together (higher spin rates will have lower angular rates and vice versa).

     

    Any more info needed then please let me know.

     

    Many Thanks,

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi DAB and Michael,

     

    Many Thanks for both of your replies.  Some more information regarding the specifications:

     

    -Device will need to be free with output via wireless transmission. (RF Transmitter?).

     

    -Everything (Sensor,Power Source, Wireless Transmitter will need to fit inside a space of no more than 40mm diameter).

     

    -Power, due to space constraint I envisiaged be supplied by some sort of button cell battery (1.5-3V?).

     

    -No cost constraints. (Yet!!)

     

    -Measurement will need to be made within approx. 0.03s of initial movement.


    -Max. Linear Acceleration - 134112m/s/s (67.1m/s in 0.0005s).

     

    -Max. Angular Acceleration - 3140000 rad/s/s (Not sure if this calculation is correct. I have assumed max. angular rate of 1570 rad/second is reached at the same time as max. linear speed)

     

    -I'm not yet sure about accuracy requirementsbut for now work on +/- 2% on all measurements.

     

    The values above are maximums and maximun linear/angular speeds will not occur together (higher spin rates will have lower angular rates and vice versa).

     

    Any more info needed then please let me know.

     

    Many Thanks,

     

    Andy.