Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensor for measuring Spin Rate/Angle & Velocity/Angle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 349 subscribers
  • Views 3871 views
  • Users 0 members are here
Related

Sensor for measuring Spin Rate/Angle & Velocity/Angle

e14 Contributor
e14 Contributor over 15 years ago

Hello All,

 

I have an application which requires a sensor to measure spin rate/angle and velocity/angle.  The spin rate can be anything from -6000 to 90000°/s  and the velocity anything up to 200mph.  I do not need to measure this over a period of time, just an instantaneous reading at a point in time.  The sensor would also need to measure the spin axis as well as the velocity in the X, Y & Z axes (or just the velocity and some way of determining the angular direction).  I have looked at MEMS Gyroscopes/Accelerometers but there does not seem to be anything out there that measures high enough values.  I have been advised that a "resolver to digital device" may work but am not entirely sure what these measure.  Can anyone please offer any assistance as to what may be a suitable product?

 

Many Thanks

 

Andy.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi,

     

    Having investigated the accelerometer/gyro options, it would seem that there is nothing really suitable to measure/withstand these forces.  I did find one accelerometer which was capable of measuring up to 20000g and withstanding up to 60000g but was single axis only.  I have found nothing in terms of a gyro to measure the spin rate needed.

     

    I am now looking at it from a different angle and considering an 'external' rather than 'embedded' sensing system which can detect/measure the required parameters.  The requirements in terms of what needs to be measured remain as per my previous posts.  I have thought possible ultrasonic sensors or some form of magnetic (Magneto-Resistive?) sensors but not sure if these would be suitable.  Does anyone have any thoughts on this?  The object that I am trying to measure is a golf ball and would like to take all the measurements as soon after initial launch (impact with golf club) as possible.

     

    Any suggestions would be most appreciated.

     

    Many Thanks,

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Aren't there systems already in existance that will take the measurments you want? I'm sure i've seen them in the higher end sporting goods stores where cameras track the club and the ball and then are able to calculate the forces involved based on the size of the ball, velocity of the swing, angle it was struck and so on. These systems are more for helping a golfer improve there swing but can be used to caculate the forces on the ball.

     

    Trying to cram everythging you wanted into a golf ball probably wasn't feasable to start with. Even if you could get it all in there the ballance and weight of the ball would be effected to the point that the measurments wouldn't reflect real world conditions on a actual golf ball.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for your reply Michael.  Yes, there are systems (simulators) available.  The issue is that the lower end models, only measure the path/angle of the club (normally with infra-red sensors) and based on that 'estimate' what the ball will do.  This leads to a large degree of inaccuracy.  If you took one of these systems to a driving range and hit a real shot, you would find that there was very little correlation between reality and simulation.  (I've done this so know what the limitations are).

     

    The camera systems are better and more accurate and tend to use a combination of very high speed cameras and infra-red technology to measure both ball and club face.  These systems tend not to measure the spin of the ball but rather the launch speed/angle using the high speed cameras and again 'estimate' the spin based on the club you have told the system you are using and the club data from the infra-red sensors.  Again, this leads to inaccuracies.

     

    The high-end systems that I have seen use either Doppler radar to track the full flight of the ball (these are the ones you may have seen on TV golf coverage when you see a 'tracer' line showing the path of the ball from behind after a player has hit a shot) or possibly laser based systems which use what I believe is termed a 'laser curtain' to measure the ball as it passes through it.  Whilst these system are the most accurate they cost tens of thousands of pounds.

     

    In my opinion, the only important thing to measure in order to accurately simulate the flight of a golf ball is to measure the 'initial' launch characteristics of the ball itself.  These launch characteristics would be the initial velocity of the ball (either in terms of a linear velocity and the angle [X & Y] at which the ball is launched, or the three component axis velocities [X, Y & Z]) and the spin rate/axis angle of rotation of the ball.  From this, using aerodynamic physics, the flight path can be calculated.

     

    So my question remains, might there be an alternative sensor system that could measure these characteristics?

     

    Many Thanks,

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 14 years ago in reply to e14 Contributor

    Hello Andy,

     

    No - there isn't anything that will do this (ie buried in the ball) for less than 10s (more like 100s k£). You are asking for a full six degree of freedom inertial tracking system perhaps 1cm cube size with radio telemetry  - the only other applications for a similar device are military and last time I knew much about what might be going on there they didn't have one either.

    High speed cameras are your best bet - if you have a few of them you can measure the intial velocity and spin of the ball.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Thanks again Michael for your reply.  Yes, it was asking a bit much to expect that sort of measurement capability embedded within the ball. Do you have any thoughts on the feasibility of using  a magneto-resistive sensor or maybe a ultra sonic sensing system to achieve the required measurements?  From the little I know about the magneto-resistive system, it would require a magnet to be embedded within the ball in order to sense it.  I believe they can be configured to measure both linear & angular velocity but one issue is that the gap between the sensor & the magnet is small (2mm- 5mm max.) from those that I have seen.  This would be too small for my application unless a system with a larger gap measurement is available.  I know nothing about the ultra-sonic sensors so whether this is feasible and worth pursuing further I do not know.  Another sensing option that I have only just come across is fibre-optics which appear to create a beam for an object to pass through but not even sure what these are intended to measure.

     

    Anyway, if you have any thoughts then please let me know.

     

    Many Thanks

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Thanks again Michael for your reply.  Yes, it was asking a bit much to expect that sort of measurement capability embedded within the ball. Do you have any thoughts on the feasibility of using  a magneto-resistive sensor or maybe a ultra sonic sensing system to achieve the required measurements?  From the little I know about the magneto-resistive system, it would require a magnet to be embedded within the ball in order to sense it.  I believe they can be configured to measure both linear & angular velocity but one issue is that the gap between the sensor & the magnet is small (2mm- 5mm max.) from those that I have seen.  This would be too small for my application unless a system with a larger gap measurement is available.  I know nothing about the ultra-sonic sensors so whether this is feasible and worth pursuing further I do not know.  Another sensing option that I have only just come across is fibre-optics which appear to create a beam for an object to pass through but not even sure what these are intended to measure.

     

    Anyway, if you have any thoughts then please let me know.

     

    Many Thanks

     

    Andy.