Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensor for measuring Spin Rate/Angle & Velocity/Angle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 2 answers
  • Subscribers 350 subscribers
  • Views 3864 views
  • Users 0 members are here
Related

Sensor for measuring Spin Rate/Angle & Velocity/Angle

e14 Contributor
e14 Contributor over 15 years ago

Hello All,

 

I have an application which requires a sensor to measure spin rate/angle and velocity/angle.  The spin rate can be anything from -6000 to 90000°/s  and the velocity anything up to 200mph.  I do not need to measure this over a period of time, just an instantaneous reading at a point in time.  The sensor would also need to measure the spin axis as well as the velocity in the X, Y & Z axes (or just the velocity and some way of determining the angular direction).  I have looked at MEMS Gyroscopes/Accelerometers but there does not seem to be anything out there that measures high enough values.  I have been advised that a "resolver to digital device" may work but am not entirely sure what these measure.  Can anyone please offer any assistance as to what may be a suitable product?

 

Many Thanks

 

Andy.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to michaelkellett

    Thanks again Michael for your reply.  Yes, it was asking a bit much to expect that sort of measurement capability embedded within the ball. Do you have any thoughts on the feasibility of using  a magneto-resistive sensor or maybe a ultra sonic sensing system to achieve the required measurements?  From the little I know about the magneto-resistive system, it would require a magnet to be embedded within the ball in order to sense it.  I believe they can be configured to measure both linear & angular velocity but one issue is that the gap between the sensor & the magnet is small (2mm- 5mm max.) from those that I have seen.  This would be too small for my application unless a system with a larger gap measurement is available.  I know nothing about the ultra-sonic sensors so whether this is feasible and worth pursuing further I do not know.  Another sensing option that I have only just come across is fibre-optics which appear to create a beam for an object to pass through but not even sure what these are intended to measure.

     

    Anyway, if you have any thoughts then please let me know.

     

    Many Thanks

     

    Andy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    SST Inclinometer Remarkable Performance-EADS successful application

     

    Shanghai, China 2012-9-5

     

    EADS and Vigor have accomplished the first stage of the cooperation agreement, and to be the sole inclinometer supplier of EADS’ subordinate company (Cassidian Company).  In June 2012,the latest patent achievement of Vigor Technology——SST300 inclinometer. Due to its excellent performance, perfect engineering and superior intelligence, the actual angel measurement accuracy concept, the SST300 stands out from many counterparts, and for this reason it is formally purchased and used by EADS. This is the second time excellent SST300 inclinometer products have been provided to European’s ordnance enterprises after Vigor provided SST400 series inclinometer products to BAE systems company; It was also after a great military application of the SST300 inclinometer that it officially launched in December 2011. Thus, Vigor inclinometer is gradually developing to become a higher application area in the international market, which changes the misconception “China's sensor can only be used in the lower-end market and lower-end project”. Furthermore, this certainly proves that China has the ability to do well in sensor products. The SST inclinometer can be set up in the high-end field of the world and also can participate in competitions with the international top market.

     

    Shanghai Vigor Technology Development Co., Ltd is a technology oriented enterprise which focuses on developing, designing and selling high tech sensor equipment with a number of patents and greatly acclaimed products in the sensor area. During the development, Vigor Technology has provided professional accurate sensor products to many scientific research projects, as well as in application fields: civil engineering, industry, military, etc. Vigor Technology's inclinometer has very great advantages over varieties of inclinometer. With its world-class   research and development ability, Vigor customizes most special requirements of its inclinometer for customers.  It also has provided year’s stability that has reached 3.6” of its ultra-high accuracy.  Their inclinometer meets products requirements of the highest security level SIL3 in the mechanical industry. The cooperation product between EADS and Vigor is the latest development of the SST300 series inclinometer.  From developing to testing all the way to the meticulous and comprehensive certification, the product’s performance and accuracy achieved a fully satisfactory level. SST300 inclinometer’s housing went through a strict modal test.  It's not simple to assemble the sensor’s core component and enclosure into products.  Also, the sensor’s PCBA also went through a modal test, fundamentally solving the effect of sensor filtering caused by the resonance of vibration. Moreover, in order to improve accuracy, Vigor Technology adopted specialized automatic testing technology to reduce man-made jamming effects to the quality, which ensures its consistency. According to the detected data, Vigor’ SST inclinometer can achieve±5″@-40~85℃ full temperature within comprehensive accuracy, and 12 months of zero stability can achieve ±3.6″.

     

    In the field of sensor technology, Vigor’s inclinometer technology has reached the leading level of the world. Beyond that, Vigor Technology ‘s sensor has many applicable advantages, which benefits from angle measuring fields that can obtain nearly 30 kinds of invention patents, utility model patents, appearance patents and software copyrights. 

     

              Due to Vigor Technology's unique advantages in the inclinometer field, many  foreign enterprises and organizations traveled to China to discuss business and have reached business agreements, and the recent cooperation with EADS has a very important significance.  Cassidian http://www.cassidian.com is known as the subsidiary of EADS, who is theglobal leader of security solution and system, to provide Lead Systems Integration, value-added products and services all over the world; that including air-conditioning systems (airplane and UAS), terrestrial systems, navy joint systems, intelligence monitoring, network security, secret communications, test systems, missiles, and service and support solutions. Cassidian has about 28000 employees, and an annual income of 5.8 billion Euros In 2011. EADS(http://www.eads.com)is the global leader of aerospace, defense and related service. In 2011, EADS grouped with an airbus company,Astrium, and a Cassidian and European helicopter company which have produced 49.1 billion Euros and have hired more than 133000 employees .

     

    The cooperation between EADS and Vigor Technology means that SST inclinometer’s quality level has reached international military field standard, which can be used in military application fields for high accuracy and reliability requirement.

    Attachments:
    imageSST Inclinometr Remarkable Performance-EADS successful application.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<