Sensors
  • Technologies
  • More
Sensors
Sensor Forum ZTP 135 SR circuit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 353 subscribers
  • Views 3128 views
  • Users 0 members are here
Related

ZTP 135 SR circuit

e14 Contributor
e14 Contributor over 15 years ago

I want to have a circuit design and how to use the sensor ZTP 135SR. I  want to apply it to measure human skin temperature and expect the output  to be voltage. I have looked at its datasheet but can not find the  connection schematic. The best I can found is here http://www.thermometrics.com/assets/images/thermopile.pdf but  it does not specify the values (R, C, V). I'm new to electronics, and I  just need a circuit to implement so any help will be welcomed.  Please be specific (like what kind of op amps, or those values), again since I'm a new comer. Many thanks.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    So the math illudes me a bit, it has been a very long time since I had to do that kind of math image

     

    but examining the circuit and assuming it works (It looks like it should), the opamp has a gain of atleast 100 or possible way more in the configuration shown, the thermopile will generate only a small voltage (mV) so the opamp is needed no matter what and the ouput of this should be sent to the micro, in the same way as the origional project did, unless you have a micro that has a gain stage that can amplify over 100* then you must use the op amp as shown int he sample schematic, your micro will nevery have enough resolution to resolve the temperaure without it. And if your doing the op amp, you may as well hook up the thermister as shown too, you can still read the thermistor output but it will automatically compensate for ambient without the micro

     

    the thermistor output range is significantly reduced by limiting its supplied voltage by strapping it across R2 which is in the middle of a resistor divider chain 1K, (R2) 200ohm, 200ohm,  and this configuration is designed to limit the compensation to a similar range as the thermocould will generate I would think.

     

    based on this code shown and the result graphs, the input to the micro is about 1V ish, so you could increase the value of R6 to maybe 200K to increase the gain and improve the overall dynamic range, could even go to perhaps a 470K if your feeding into a 5V controller and the reference is set to the VCC (Default on an UNO), remember the PIC will have been using a different VREF that equates to the 1023 reading so you will have to adjust the value when running on the Yun

     

    the code clearly shows the math involved and would require very little change to get it working from the PIC it was written for, there bot C and to get the LCD working you would just replace it with the approprite library

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • garypty
    0 garypty over 8 years ago in reply to Robert Peter Oakes

    I know this post is more than three years ago, but I have a similar issue. The hyper-link above are broken. Could you kindly show the schematics that you are talking about? Thank you very much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • garypty
    0 garypty over 8 years ago in reply to Robert Peter Oakes

    I know this post is more than three years ago, but I have a similar issue. The hyper-link above are broken. Could you kindly show the schematics that you are talking about? Thank you very much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • qaibou
    0 qaibou over 8 years ago in reply to garypty

    Me too, I have the same problem, I can't open them and I don't have enough information about this sensor