Sensors
  • Technologies
  • More
Sensors
Sensor Forum Sensors used on faucets, trashcans, etc.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 351 subscribers
  • Views 831 views
  • Users 0 members are here
  • infrared_switch
  • proximity_sensors
  • ap:sensor
  • faucet
Related

Sensors used on faucets, trashcans, etc.

e14 Contributor
e14 Contributor over 13 years ago

I have a new use for the reflective infrared sensors used on automatic lavatory faucets and the self-opening lids on trashcans. (Hold your hand in front of it to activate.)

 

I've been looking for a module for under $20, battery operated for long periods with 3 - 12 VDC, sensing distance of 2" - 4" (50mm-100mm).

 

Incident sunlight is not an issue; it would be used in a covered area. I need a discrete wired package that I can handle and mount, not SMD's.

 

Can you recommend an online source & part number? Everything I find is either for shorter or longer sensing ranges, far too expensive ($75+), out of stock, etc. I just want the same part they use in faucets and trashcans (they're everywhere).

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 13 years ago

    http://img.alibaba.com/img/pb/519/060/507/507060519_403.jpghttp://www.newark.com/jsp/displayProduct.jsp?sku=33C1109&CMP=KNC-G-SKU-Vishay&mckv=si1z4vqfy|pcrid|13938172701|plid|

     

    These can be had for about $0.18 each but look at the external part$ count!  Just like some projects benefit from multiplexed LED outputs, I think these will need multiplexed input processing.  I am thinking like when they are placed all around the perimeter of a mobile robot.  But, how does one do that most effectively within the Hardware/Software Continuum of Design Choices?  Thanks for bringing this up - it stimulated my thinking.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    Thank you, Billabott, but that device only works at a distance of 2mm (about 1/8 of an inch). I need to go from 100mm to 200mm (4" to 8") sensing range.

     

    What else ya got?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    Thank you, Billabott, but that device only works at a distance of 2mm (about 1/8 of an inch). I need to go from 100mm to 200mm (4" to 8") sensing range.

     

    What else ya got?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Murata is the industry leader.  They have probably made a breakthrough of some type but are only selling it to manufacturers for now.  Maybe some day in the distant future you can buy the one you want at Radio Shack.  Here is a clue of their new  tech: http://www.computerworld.com/s/article/9231980/Tiny_sensor_allows_gesture_control_of_tablets_phones

     

     

    One of the touchless faucets on Amazon.com used 4 AA batteries.  So that is 6 volts.  The only way I can think of is that it uses Fresnel lens.  One for the emitter(s) and one for the detector.  If you put an object at the intersection of the two beam paths then you can get an activation.  That is how the PIRs are able to detect motion in their field of view.   But you knew that, didn't you?

     

    Moving up to: The Parallax Radio Frequency Identification (RFID) Read/Write Module provides a low-cost solution to read and write passive RFID transponder tags up to 3 inches away.

     

    Next step up: Ultrasound echo range finder.  image

    http://www.amazon.com/Virtuabotix-Ultrasonic-Distance-Rangefinder-Detection/dp/B0066X9V5K/ref=sr_1_2?ie=UTF8&qid=1357218870&sr=8-2&keywords=arduino+range+finder