Sensors
  • Technologies
  • More
Sensors
Sensor Forum Digitally Addressable Sensors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 351 subscribers
  • Views 2498 views
  • Users 0 members are here
  • sensors
  • sensor
Related

Digitally Addressable Sensors?

amillen
amillen over 13 years ago

I need to come up with a way to daisy chain a number of sensors together and uniquely read the high/low pin from them individually. Think Digital RGB LED http://www.adafruit.com/products/306 or I2C. I like how when you power the LED strip up, it assigns a unique id. Is there already a module that will do this?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hi Alex, With I2C you can chain only upto 128 devices/sensors. This is the caveat. If you have more than 128 devices/sensor you need to use I2C chips like wherein you can theorotically connect NXP/Phillips…
  • amillen
    amillen over 12 years ago +1 verified
    Thanks to all that replied, many of you came up with different solutions, but I was looking for something a little more off the shelf. Looks like someone finally packaged up exactly what I was looking…
Parents
  • vsluiter
    0 vsluiter over 13 years ago

    Hello Alex,

    To accomplish what you want, you'd need something that is daisychained, or at least have a chain of devices where the first in the chain can 'disable' all others. I2C , without modifications or other circuitry, won't be able to do what you want. As it is a bus-topology, all devices are being 'talked to' at the same time, and all devices with the same address will respond simultaneously, thus causing bus collisions.

    You'd either need a device with an 'ingoing' and 'outgoing' bus, or something that disables all other devices until it is being addressed. In both cases you could do this with a simple microcontroller. Which is of course the kind of work you're not waiting for image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 13 years ago

    Hello Alex,

    To accomplish what you want, you'd need something that is daisychained, or at least have a chain of devices where the first in the chain can 'disable' all others. I2C , without modifications or other circuitry, won't be able to do what you want. As it is a bus-topology, all devices are being 'talked to' at the same time, and all devices with the same address will respond simultaneously, thus causing bus collisions.

    You'd either need a device with an 'ingoing' and 'outgoing' bus, or something that disables all other devices until it is being addressed. In both cases you could do this with a simple microcontroller. Which is of course the kind of work you're not waiting for image