Sensors
  • Technologies
  • More
Sensors
Sensor Forum Digitally Addressable Sensors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 351 subscribers
  • Views 2496 views
  • Users 0 members are here
  • sensors
  • sensor
Related

Digitally Addressable Sensors?

amillen
amillen over 13 years ago

I need to come up with a way to daisy chain a number of sensors together and uniquely read the high/low pin from them individually. Think Digital RGB LED http://www.adafruit.com/products/306 or I2C. I like how when you power the LED strip up, it assigns a unique id. Is there already a module that will do this?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hi Alex, With I2C you can chain only upto 128 devices/sensors. This is the caveat. If you have more than 128 devices/sensor you need to use I2C chips like wherein you can theorotically connect NXP/Phillips…
  • amillen
    amillen over 12 years ago +1 verified
    Thanks to all that replied, many of you came up with different solutions, but I was looking for something a little more off the shelf. Looks like someone finally packaged up exactly what I was looking…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Alex,

     

    SPI can be daisy chained, although the specific slave device has to support it, and its not always immediately obvious if it does or not.

     

    What sort of sensor are you considering?  you mention a high/low pin, so that's digital inputs then?  something like the MCP23S17 possibly?

     

    You should give this a read : http://www.maximintegrated.com/app-notes/index.mvp/id/3947

     

    Best regards,

    Charlie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 13 years ago in reply to e14 Contributor

    Charlie,

    The example you gave is interesting, but (at least the examples) only apply to output devices, not inputs. The MCP23S17 does not mention daisy chaining in its datasheet.

    If Alex is still alive (haven't seen any reaction since the original post), he might do this: read through the datasheet of the WS2811 to understand how to do daisy chain addressing[pdf], and get a free LPC800 board to implement the same protocol image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to vsluiter

    Victor,

     

    The OP mentioned "uniquely read the high/low pin from them individually" which I interpret as an input. I agree that the MCP23S17 datasheet doesn't specifically mention daisychaining, and quite possibly its not possible with that particular chip, but I was attempting to discover what sort of sensors he means, whether digital input, analogue (ADC/temperature/pressure etc) or whatever.

    I've personally used 40 MCP23S17 chips in a single solution, although there I used 5 CS signals for each group of 8 addressed chips, with a common CLK/SI/SO across all 40, for a total of 8 lines. 40 chips at 16 I/O per chip=640 I/O channels image

     

    It occurs to me that maybe a topology like that would be sufficient for Alex?  I know that doesn't specifically answer his daisychaining question, but sometimes its easy to accidentally make assumptions in an original question.

     

    I hope Alex IS still alive....

     

    Best regards,

    Charlie.

     

    p.s. I just looked again at the MCP23S17 datasheet. I think that the SPI input timing diagram (Figure 2-5 on page 32) shows that this particular device is not suitable for daisychaining, because the data coming into SI is not copied to SO. I've used other SPI devices which do exhibit that behaviour though.

     

    p.p.s. I may look into the free LPC800 board you mentioned. As ever its finding the time...

     

     

    p.p.p.s Here's an example of an IO expander using SPI which can be daisychained : http://datasheets.maximintegrated.com/en/ds/MAX7317.pdf   Mind you, the datasheet gives a limit of 10 on a single chain because of propagation delays of SI/SO versus CLK. Hmmm... Maybe SPI daisychaining isn't the way to go....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to vsluiter

    Victor,

     

    The OP mentioned "uniquely read the high/low pin from them individually" which I interpret as an input. I agree that the MCP23S17 datasheet doesn't specifically mention daisychaining, and quite possibly its not possible with that particular chip, but I was attempting to discover what sort of sensors he means, whether digital input, analogue (ADC/temperature/pressure etc) or whatever.

    I've personally used 40 MCP23S17 chips in a single solution, although there I used 5 CS signals for each group of 8 addressed chips, with a common CLK/SI/SO across all 40, for a total of 8 lines. 40 chips at 16 I/O per chip=640 I/O channels image

     

    It occurs to me that maybe a topology like that would be sufficient for Alex?  I know that doesn't specifically answer his daisychaining question, but sometimes its easy to accidentally make assumptions in an original question.

     

    I hope Alex IS still alive....

     

    Best regards,

    Charlie.

     

    p.s. I just looked again at the MCP23S17 datasheet. I think that the SPI input timing diagram (Figure 2-5 on page 32) shows that this particular device is not suitable for daisychaining, because the data coming into SI is not copied to SO. I've used other SPI devices which do exhibit that behaviour though.

     

    p.p.s. I may look into the free LPC800 board you mentioned. As ever its finding the time...

     

     

    p.p.p.s Here's an example of an IO expander using SPI which can be daisychained : http://datasheets.maximintegrated.com/en/ds/MAX7317.pdf   Mind you, the datasheet gives a limit of 10 on a single chain because of propagation delays of SI/SO versus CLK. Hmmm... Maybe SPI daisychaining isn't the way to go....