Sensors
  • Technologies
  • More
Sensors
Sensor Forum Digitally Addressable Sensors?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 351 subscribers
  • Views 2498 views
  • Users 0 members are here
  • sensors
  • sensor
Related

Digitally Addressable Sensors?

amillen
amillen over 13 years ago

I need to come up with a way to daisy chain a number of sensors together and uniquely read the high/low pin from them individually. Think Digital RGB LED http://www.adafruit.com/products/306 or I2C. I like how when you power the LED strip up, it assigns a unique id. Is there already a module that will do this?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hi Alex, With I2C you can chain only upto 128 devices/sensors. This is the caveat. If you have more than 128 devices/sensor you need to use I2C chips like wherein you can theorotically connect NXP/Phillips…
  • amillen
    amillen over 12 years ago +1 verified
    Thanks to all that replied, many of you came up with different solutions, but I was looking for something a little more off the shelf. Looks like someone finally packaged up exactly what I was looking…
Parents
  • amillen
    0 amillen over 13 years ago

    Yes, Alex is still alive, sorry for the delay in my response. I'm still digesting all of the information I have received and would like to respond to some of your questions.

     

    I'm reading (input), anywhere from 1 to 20 snap or magnetic switches.

     

    The same project but different application, I have 1 to 20 analog sensors http://www.parallax.com/tabid/768/ProductID/100/Default.aspx

     

    I will never be daisychaining both sensors on the same chain, either one or the other, and am willing to have two different solutions.

     

    The desire to daisychain instead of running separate lines, is that the user will be adding and subtracting sensors often.

     

    I hope that answers some questions, let me know if you have anymore and I will answer them while I read over all this info

     

    Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • amillen
    0 amillen over 13 years ago

    Yes, Alex is still alive, sorry for the delay in my response. I'm still digesting all of the information I have received and would like to respond to some of your questions.

     

    I'm reading (input), anywhere from 1 to 20 snap or magnetic switches.

     

    The same project but different application, I have 1 to 20 analog sensors http://www.parallax.com/tabid/768/ProductID/100/Default.aspx

     

    I will never be daisychaining both sensors on the same chain, either one or the other, and am willing to have two different solutions.

     

    The desire to daisychain instead of running separate lines, is that the user will be adding and subtracting sensors often.

     

    I hope that answers some questions, let me know if you have anymore and I will answer them while I read over all this info

     

    Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to amillen

    Alex,

     

    I think I'm starting to see what you're getting at. with the discrete inputs (the switches), will there be (say) 20 sockets into which a switch may or may not be connected or should I think more like an ethernet arrangement where each switch is completely self-contained, and if there's no switch then there's not even a socket for the switch?

     

    For the QTI sensor (looks interesting BTW), same question I suppose. Also, what sort of analogue resolution would you need? (just thinking about ADC method)

     

    You may consider one or more PIC devices, some of which have multiple analogue inputs. If the sensor nodes are to be self-contained, then each node could contain a PIC (they're relatively cheap) which themselves provide/support SPI/I2C (or maybe a UART chain?) to connect the chain. There'd be a little programming needed for the PICs, but each node would only require fairly simple logic. If you're not familiar with PICs, start by looking at the PIC16F886. I'm not saying that's the one to use, just a stating point. In reality you'd probably want a smaller (less pins) PIC. THere are plenty of examples of programming PICs available.

     

    Best regards,

    Charlie.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • danteo
    0 danteo over 13 years ago in reply to amillen

    Hi Alex,

     

    Take a look at this 1-wire network guidelines too:

    http://www.maximintegrated.com/app-notes/index.mvp/id/148

     

    Here is a reference schematic:

    http://www.maximintegrated.com/app-notes/index.mvp/id/244

     

    Hope it helps,

    Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer