Sensors
  • Technologies
  • More
Sensors
Sensor Forum Hydroponic system nutrient sensors help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 15 answers
  • Subscribers 361 subscribers
  • Views 7697 views
  • Users 0 members are here
Related

Hydroponic system nutrient sensors help

xan326
xan326 over 13 years ago

Hi all, I'm going to be building a hydroponic system soon being controlled and monitored by a board (most likely beaglebone). But I need help with finding sensors and connecting them, I have literally no idea what connect tivity any boards have (rasberry pi, arduino, beaglebone/beagleboard, atmel) and if they're just USB, then finding a way to convert connections to usb. But I'll get into that later.

The sensors I need are:

Dissolved Oxygen

Hydrogen

Carbon

Nitrogen

Potassium

Phosphorus

Calcium

Magnesium

Sulfur

Boron

Chlorine

Copper

Iron

Molybdenum

Manganese

Zinc

Nickel

Sodium

Cobalt

Selenium

Silicon

Then PH and Flow rate sensors

 

Anyways, if anyone knows of any place to get these sensors please tell me or post a link. Also if they're not natively USB, explain a way (or post a link to an article) on how to convert the connection to usb.

Thanks to everyone that will help! This is my first project using any of the boards like beagle or arduino.

 

Also does anyone know of any pumps; both air and water; that can be run from one of the boards?

  • Sign in to reply
  • Cancel

Top Replies

  • davewr
    davewr over 13 years ago in reply to xan326 +1 suggested
    Just one more note -- if you consider the question answered - mark it as answered as a courtesy to me and to everyone reading the thread. If you have more questions start a new thread with specific questions…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have a lot of experience in Hydroponics, I have designed hydroponic solutions from the ground up and done testing on them. Daniel is right you dont need to monitor everything you have listed. You have listed all the major components was well as all the micro-nutrients needed to maintain the plants. All you have to do is monitor the PH and TDS in solution and simply flush and re-new as needed.

     

    However, if you are trying to monitor an experiment and determine the uptake of given nutrients within solution so you can simply add back what was removed. You are looking for a spectrophotometer which you would need to make and interface to any of the micro-controllers. You would use it to do Absorption spectroscopy on the solution. Samples could be diverted from the main flow line into a secondary line for testing then released back into the main flow line after the test. Most spectrophotometers use a cuvette for sample preparation. These tend to be plastic but in the case of UV spectroscopy they are quartz. You would have to look up each of the chemicals you list and determine what spectrum they absorb. You would also need to make sure that the sample test area is made of a material that will not absorb the spectrum you are trying to identify. If any of them are in the UV spectrum then you will need to use quartz at the sample point and the design gets much more complicated.

     

    None of this is easy or simple, I would suggest that you stick to the standard PH/TDS tests unless you are up for a challenge. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have a lot of experience in Hydroponics, I have designed hydroponic solutions from the ground up and done testing on them. Daniel is right you dont need to monitor everything you have listed. You have listed all the major components was well as all the micro-nutrients needed to maintain the plants. All you have to do is monitor the PH and TDS in solution and simply flush and re-new as needed.

     

    However, if you are trying to monitor an experiment and determine the uptake of given nutrients within solution so you can simply add back what was removed. You are looking for a spectrophotometer which you would need to make and interface to any of the micro-controllers. You would use it to do Absorption spectroscopy on the solution. Samples could be diverted from the main flow line into a secondary line for testing then released back into the main flow line after the test. Most spectrophotometers use a cuvette for sample preparation. These tend to be plastic but in the case of UV spectroscopy they are quartz. You would have to look up each of the chemicals you list and determine what spectrum they absorb. You would also need to make sure that the sample test area is made of a material that will not absorb the spectrum you are trying to identify. If any of them are in the UV spectrum then you will need to use quartz at the sample point and the design gets much more complicated.

     

    None of this is easy or simple, I would suggest that you stick to the standard PH/TDS tests unless you are up for a challenge. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer